cancel
Showing results for 
Search instead for 
Did you mean: 

X-Nucleo-GFX01M1 GUI extension support Nucleo-G070RB?

Kkanu.1
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi,

What is your question exactly ? Does the Nucleo-G070RB supports the X-Nucleo-GFX01K1 display ? If yes, then it does. Since you added the TouchGFX tag I suppose you are wondering if it will work with TouCHGFX ? The answer is also yes, but there are no application templates available in TouchGFX Designer. You can have a look at the application template for the STM32G071-nucleo board, which uses the X-Nucleo-GFX01K1 display, and use it to configure your project.

/Romain

View solution in original post

3 REPLIES 3
Romain DIELEMAN
ST Employee

Hi,

What is your question exactly ? Does the Nucleo-G070RB supports the X-Nucleo-GFX01K1 display ? If yes, then it does. Since you added the TouchGFX tag I suppose you are wondering if it will work with TouCHGFX ? The answer is also yes, but there are no application templates available in TouchGFX Designer. You can have a look at the application template for the STM32G071-nucleo board, which uses the X-Nucleo-GFX01K1 display, and use it to configure your project.

/Romain

Kkanu.1
Associate

KK.Thank you.

Alexandre RENOUX
Principal

Hello Kkanu.1,

When your question is answered, please close this topic by choosing Select as Best.

/Alexandre