2022-02-15 07:48 AM
2022-02-16 01:17 AM
Hello DOliv.1,
We're sorry for the inconvenience. Can you share your log file please ? (the path for it is : C:\Users\YOUR_USER_NAME\AppData\Roaming\TouchGFX-4.18.1\TouchGFXDesigner.log) I'll try to have a look.
Meantime, I can suggest you to reinstall your TouchGFX Designer and retry.
/Osman
2022-02-16 01:25 AM
Hi Osman,
thanks for your answer.
Here attached you’ll find the log.
I’ve already tried to reinstall the software, but I’ve got the same error.
Thanks in advance.
2022-02-16 04:05 AM
Hi DOliv.1,
Can you share the log file through the forum please ? :)
(I think sharing files by mail doesn't work)
Also, a colleague told me maybe you can try to open Microsoft Edge before and after your TouchGFX Designer, he had a similar bug, and this is just to make sure you have access to our servers.
/Osman
2022-02-16 05:31 AM
2022-02-16 05:33 AM
P.S. Opening Microsoft Edge before TouchGFX Designer has no result.
2022-02-17 02:13 AM
Hi DOliv.1,
I analyzed your log file, there is a TLS alert: 'HandshakeFailure'. I might be due to your Windows version. Which version do you use ?
Indeed, we don't support Windows 7 and Windows 8 anymore in our newest versions, so if you use w7 or w8, I recommend you to use older version of TouchGFX Designer.
Also, can you try to create a project in a TouchGFX Designer 4.17.0 for example (not under 4.16), and open it with your TGFX Designer 4.18.1 ?
/Osman