2019-09-13 3:00 AM
Hi @Martin KJELDSEN !
This time I'm trying to make a scrollable container containing custom containers I've made. But how do I add the custom container to be a part of the scrollable container in the designer? I can't get the scrollable container to scroll when I first add a scrollable container and then add my custom containers. And I tried making a custom container with a scrollable container, but then I can't add my custom container to my other custom container including the scrollable container. Do you follow? :grinning_face_with_sweat:
Do you have any examples using scrollable containers that can inspire me to solve my issue? Preferrably examples I can open in the designer. :smiling_face_with_smiling_eyes:
Thankful for answers!
Solved! Go to Solution.
2019-09-16 4:28 AM
Hi @Sandy.Dahl ,
Here's a simple example. I created two large custom containers that contain a box each (gree and red, respectively). I added those to the scrollable container by simply dragging them from the project overview (after adding them to canvas) into scrollablecontainer1.
I made the canvas look like this:
And i can now drag the list containing the two elements:
2019-09-16 4:28 AM
Hi @Sandy.Dahl ,
Here's a simple example. I created two large custom containers that contain a box each (gree and red, respectively). I added those to the scrollable container by simply dragging them from the project overview (after adding them to canvas) into scrollablecontainer1.
I made the canvas look like this:
And i can now drag the list containing the two elements:
2019-09-16 5:23 AM
Oh, that was simple, I tried adding the containers by clicking on them. Thanks!
2019-09-16 6:22 AM
Nice. No problem! :)
/Martin