2025-02-13 2:38 PM
Hi everybody,
I have some screens where is present a scrollable container and listLayout like child to generale a scrollable list (in other words a vertical menu) (see the video).
Everytime I scroll Up e Down the container a glitch compare in the middle of screen like a horizontal black line.
The project has a lot of screen but I don't have any other problems with transictions or other objects.
Only with scroll container in every page their are present..
I'm using a custom board with an STM32H743VIT6 and a 16bit RGB display. connected on LTDC.
(all graphic assets are placed into an external QSPI memory )
I tried to disable DMA2D, Dcache, I change the clock of LTDC but without success.
Does someone has some ideas? some suggestion?
Thanks in advance
2025-03-04 3:29 AM
I solved this problem: is not a problem caused by TouchGFX,LTDC or STM32.
It was caused by a "***" LCD that require a lot of parameters to manage it: some of them was setted wrong by myself.
After the correction everything works perfectly.
2025-03-04 6:59 AM
Hi @MPast.1
"After the correction everything works perfectly."
Could you possible share what (combination of) parameters were to blame ? I am observing a similar glitch on my display.
Thanks
2025-03-05 11:34 AM
My project is composed a display that has st7796 controller. This display (with integrated controlled) by default start working on SPI and not on RGB parallel lines.
So I need to
the original init:
// Command Set Control - enable command 2 part I
LCD_IO_WriteCmd(ST7796_CSCON);
LCD_IO_WriteData(0xC3);
// Command Set Control - enable command 2 part II
LCD_IO_WriteCmd(ST7796_CSCON);
LCD_IO_WriteData(0x96);
// Interface Mode Control
LCD_IO_WriteCmd(ST7796_IFMODE);
LCD_IO_WriteData(0x82);
// Display Inversion Control
LCD_IO_WriteCmd(ST7796_INVCTR);
LCD_IO_WriteData(0x01);
// Display Function Control
LCD_IO_WriteCmd(ST7796_DFUNCTR);
LCD_IO_WriteData(0x20);
LCD_IO_WriteData(0x02);
LCD_IO_WriteData(0x3B);
if (Orientation == PORTRAIT_0) // display TOP = NTC probe Side
{
GT911.Orientation = PORTRAIT_0;
LCD_IO_WriteCmd(ST7796_MADCTL);
LCD_IO_WriteData(0x48); //48
}
if (Orientation == PORTRAIT_180) // display TOP = smartcard side
{
GT911.Orientation = PORTRAIT_180;
LCD_IO_WriteCmd(ST7796_MADCTL);
LCD_IO_WriteData(0x88);
}
// // Display Function Control
// LCD_IO_WriteCmd(ST7796_BPC);
// LCD_IO_WriteData(0x0D); // vertical front porch period
// LCD_IO_WriteData(0x04); // vertical back porch period
// LCD_IO_WriteData(0x00);
// LCD_IO_WriteData(0x1E); // horizontal back porch period (30pixel)
// //Power Control 1
// LCD_IO_WriteCmd(ST7796_PWCTR1);
// LCD_IO_WriteData(0xF0);
// LCD_IO_WriteData(0x35);
//
// // Power Control 2
// LCD_IO_WriteCmd(ST7796_PWCTR2);
// LCD_IO_WriteData(0x15);
// Power Control 3
LCD_IO_WriteCmd(ST7796_PWCTR3);
LCD_IO_WriteData(0xA7);
// LCD_IO_WriteCmd(0xC3);
// LCD_IO_WriteData(0x09);
// VCOM Control
LCD_IO_WriteCmd(ST7796_VMCTR1);
LCD_IO_WriteData(0x25);
// Vcom Offset Register
LCD_IO_WriteCmd(ST7796_VCM);
LCD_IO_WriteData(0x00);
// negative gamma control
LCD_IO_WriteCmd(0xE8);
LCD_IO_WriteData(0x40);
LCD_IO_WriteData(0x82);
LCD_IO_WriteData(0x07);
LCD_IO_WriteData(0x18);
LCD_IO_WriteData(0x27);
LCD_IO_WriteData(0x0a);
LCD_IO_WriteData(0xb6);
LCD_IO_WriteData(0x33);
// positive gamma control
LCD_IO_WriteCmd(ST7796_GMCTRP1); //0xE0
LCD_IO_WriteData(0xD0);
LCD_IO_WriteData(0x04);
LCD_IO_WriteData(0x0D);
LCD_IO_WriteData(0x11);
LCD_IO_WriteData(0x13);
LCD_IO_WriteData(0x2B);
LCD_IO_WriteData(0x3F);
LCD_IO_WriteData(0x54);
LCD_IO_WriteData(0x4C);
LCD_IO_WriteData(0x18);
LCD_IO_WriteData(0x0D);
LCD_IO_WriteData(0x0B);
LCD_IO_WriteData(0x1F);
LCD_IO_WriteData(0x23);
// negative gamma control
LCD_IO_WriteCmd(ST7796_GMCTRN1); //0xE1
LCD_IO_WriteData(0xD0);
LCD_IO_WriteData(0x04);
LCD_IO_WriteData(0x0C);
LCD_IO_WriteData(0x11);
LCD_IO_WriteData(0x13);
LCD_IO_WriteData(0x2C);
LCD_IO_WriteData(0x3F);
LCD_IO_WriteData(0x44);
LCD_IO_WriteData(0x51);
LCD_IO_WriteData(0x2F);
LCD_IO_WriteData(0x1F);
LCD_IO_WriteData(0x1F);
LCD_IO_WriteData(0x20);
LCD_IO_WriteData(0x23);
LCD_IO_WriteCmd(ST7796_CSCON);
LCD_IO_WriteData(0x3C);
LCD_IO_WriteCmd(ST7796_CSCON);
LCD_IO_WriteData(0x69);
the final init:
// Command Set Control - enable command 2 part I
LCD_IO_WriteCmd(ST7796_CSCON);
LCD_IO_WriteData(0xC3);
// Command Set Control - enable command 2 part II
LCD_IO_WriteCmd(ST7796_CSCON);
LCD_IO_WriteData(0x96);
if (Orientation == PORTRAIT_0)
{
GT911.Orientation = PORTRAIT_0;
LCD_IO_WriteCmd(ST7796_MADCTL);
LCD_IO_WriteData(0x5C);
}
if (Orientation == PORTRAIT_180)
{
GT911.Orientation = PORTRAIT_180;
LCD_IO_WriteCmd(ST7796_MADCTL);
LCD_IO_WriteData(0x48);
}
LCD_IO_WriteCmd(ST7796_FRMCTR1);
LCD_IO_WriteData(0x82);
// Interface Mode Control
LCD_IO_WriteCmd(ST7796_IFMODE);
LCD_IO_WriteData(0x82);
// Display Inversion Control
LCD_IO_WriteCmd(ST7796_INVCTR);
LCD_IO_WriteData(0x00);
// Display Function Control
LCD_IO_WriteCmd(ST7796_DFUNCTR);
LCD_IO_WriteData(0xA0);
LCD_IO_WriteData(0x60); //0x02
LCD_IO_WriteData(0x3B);
// Power Control 3
LCD_IO_WriteCmd(ST7796_PWCTR3);
LCD_IO_WriteData(0xA7);
// VCOM Control
LCD_IO_WriteCmd(ST7796_VMCTR1);
LCD_IO_WriteData(0x25);
// Vcom Offset Register
LCD_IO_WriteCmd(ST7796_VCM);
LCD_IO_WriteData(0x00);
// Display Output Ctrl Adjust
LCD_IO_WriteCmd(0xE8);
LCD_IO_WriteData(0x40);
LCD_IO_WriteData(0x8A);
LCD_IO_WriteData(0x00);
LCD_IO_WriteData(0x00);
LCD_IO_WriteData(0x29);
LCD_IO_WriteData(0x19);
LCD_IO_WriteData(0xA5);
LCD_IO_WriteData(0x33);
// positive gamma control
LCD_IO_WriteCmd(ST7796_GMCTRP1); //0xE0
LCD_IO_WriteData(0xD0);
LCD_IO_WriteData(0x04);
LCD_IO_WriteData(0x0D);
LCD_IO_WriteData(0x11);
LCD_IO_WriteData(0x13);
LCD_IO_WriteData(0x2B);
LCD_IO_WriteData(0x3F);
LCD_IO_WriteData(0x54);
LCD_IO_WriteData(0x4C);
LCD_IO_WriteData(0x18);
LCD_IO_WriteData(0x0D);
LCD_IO_WriteData(0x0B);
LCD_IO_WriteData(0x1F);
LCD_IO_WriteData(0x23);
// negative gamma control
LCD_IO_WriteCmd(ST7796_GMCTRN1); //0xE1
LCD_IO_WriteData(0xD0);
LCD_IO_WriteData(0x04);
LCD_IO_WriteData(0x0C);
LCD_IO_WriteData(0x11);
LCD_IO_WriteData(0x13);
LCD_IO_WriteData(0x2C);
LCD_IO_WriteData(0x3F);
LCD_IO_WriteData(0x44);
LCD_IO_WriteData(0x51);
LCD_IO_WriteData(0x2F);
LCD_IO_WriteData(0x1F);
LCD_IO_WriteData(0x1F);
LCD_IO_WriteData(0x20);
LCD_IO_WriteData(0x23);
LCD_IO_WriteCmd(ST7796_CSCON);
LCD_IO_WriteData(0x3C);
LCD_IO_WriteCmd(ST7796_CSCON);
LCD_IO_WriteData(0x69);
the big problem was :
// Display Function Control
LCD_IO_WriteCmd(ST7796_DFUNCTR);
LCD_IO_WriteData(0x20);
LCD_IO_WriteData(0x02);
LCD_IO_WriteData(0x3B);the data generated by LTDC was sent to internal ST7796 controller registers instead of sent to display directly. This problem caused glitches: the original mode was not fast enough
2025-03-06 1:28 AM
Making container cachable can increase performance. And, do not forget clear cache area if you are using MPU.