cancel
Showing results for 
Search instead for 
Did you mean: 

Warning: This IP has no parameter to be configured.

FKafi.1
Associate II

When i enable STM32-XCUBE-TOUCHGFX pack in my cubeMX software ; i have no parameter to configure but i got this warning : "This IP has no parameter to be configured" .

How should i solve this issue?

0693W000000UXOBQA4.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
Khouloud ZEMMELI
ST Employee

​Try to re-install the cubemx 5.6.0 then re-check please.

View solution in original post

13 REPLIES 13
TDK
Guru

I think CubeMX is just letting you know there are no user-configurable parameters for that option. It's informational and not something that should cause problems generating or running code.

If you feel a post has answered your question, please click "Accept as Solution".
FKafi.1
Associate II

Normally, I should see something like this in configuration window :

0693W000000UaSuQAK.jpg

Khouloud ZEMMELI
ST Employee

​Hello @FKafi.1​ ,

This's a new behavior you mean ?  using which CubeMX version your latest screenshot ?

Thanks,

Khouloud

FKafi.1
Associate II

Hello @Khouloud ZEMMELI​ ;

No, it's not new. It's the first time i'm going to use this option.

My cubeMx version is 5.6.0.

Khouloud ZEMMELI
ST Employee

​Okey, I did not reproduce the issue so could you please share your ioc file?

Thanks,

Khouloud

FKafi.1
Associate II

@Khouloud ZEMMELI​ 

here is the ioc file :

​Your project is ok, there's no problem.

So why i get this warning?!!!

Khouloud ZEMMELI
ST Employee

​Try to re-install the cubemx 5.6.0 then re-check please.