2020-03-23 9:58 AM
When i enable STM32-XCUBE-TOUCHGFX pack in my cubeMX software ; i have no parameter to configure but i got this warning : "This IP has no parameter to be configured" .
How should i solve this issue?
Solved! Go to Solution.
2020-03-24 4:37 AM
Try to re-install the cubemx 5.6.0 then re-check please.
2020-03-23 10:40 AM
I think CubeMX is just letting you know there are no user-configurable parameters for that option. It's informational and not something that should cause problems generating or running code.
2020-03-24 1:24 AM
Normally, I should see something like this in configuration window :
2020-03-24 1:30 AM
Hello @FKafi.1 ,
This's a new behavior you mean ? using which CubeMX version your latest screenshot ?
Thanks,
Khouloud
2020-03-24 1:47 AM
Hello @Khouloud ZEMMELI ;
No, it's not new. It's the first time i'm going to use this option.
My cubeMx version is 5.6.0.
2020-03-24 2:09 AM
Okey, I did not reproduce the issue so could you please share your ioc file?
Thanks,
Khouloud
2020-03-24 3:27 AM
2020-03-24 3:58 AM
Your project is ok, there's no problem.
2020-03-24 4:22 AM
So why i get this warning?!!!
2020-03-24 4:37 AM
Try to re-install the cubemx 5.6.0 then re-check please.