cancel
Showing results for 
Search instead for 
Did you mean: 

Using SD card in TouchGFX/FreeRTOS project

Louie88
Senior

Hello,

I created an app form my STM32H7474I-DISCO board to test SD card based on this example. I spent a couple of hours with porting it to H747I-DISCO board, but finally it worked: I could save and load a file from an SD Card.

I implemented the whole thing into my TouchGFX based project on same discovery board. I could build and run the project but when I tried to write a new file the SD Card was mounted fine but creating a new file failed with FR_NOT_READY (The physical drive cannot work) error.

uint32_t byteswritten; if(f_mount(&SDFatFS, (TCHAR const*)SDPath, 0) != FR_OK) { Error_Handler(); } else { //Open file for writing (Create) if(f_open(&SDFile, "STM32.TXT", FA_CREATE_ALWAYS | FA_WRITE) != FR_OK) { Error_Handler(); } else { //Write to the text file res = f_write(&SDFile, wtext, strlen((char *)wtext), (void *)&byteswritten); if((byteswritten == 0) || (res != FR_OK)) { Error_Handler(); } else { f_close(&SDFile); } } }

The same code, the same development board, the same SD card works fine if I have no TouchGFX nor FreeTOS. Is this some initializing/usage error or the same code cannot be run under TouchGFX nor FreeTOS?

Thanks,
Louis

1 ACCEPTED SOLUTION
2 REPLIES 2