Skip to main content
ST AME Support NF
ST Employee
Sep 24, 2021 7:17 AM UTC

How to create a file system on an SD card using STM32CubeIDE

Introduction

Data logging applications require storing large amounts of data over a period of time. SD cards are a convenient solution for storing data and many STM32 products include the proper hardware interface. Using a standard file system to write data on an SD card ensures that the data is easily accessible on another device or computer. Adding a file system along with an SD card driver is easy to do using the various ST tools available for the STM32 family of microcontrollers.

This article details the process of configuring the SDMMC peripheral for accessing an SD card and configuring the FatFs middleware to create a file system using STM32 and ST toolsets.

Note that this article is also available in video form: STM32 – Creating a file system on an SD card - YouTube
 

Prerequisites

STM32 Discovery kits as well as evaluation boards include an SD card socket. While this example uses the STM32F746G-DISCO board, any other STM32 board with an SD card socket can be used. Ensure appropriate changes are made in the software configuration to accommodate a different target board.


1781.png

 

1. Implementation steps

1.1 Create and open STM32CubeIDE project

Firstly, we need to create a STM32CubeIDE project where we configure the application to interface with the SD card.

  1. Open STM32CubeIDE, and create a new STM32 project, selecting the STM32F746G-DISCO template.pepfof_2-1755096131183.png
  2. Give a name to your project and then click finish.1783.png
  3. Select [No] for the Board Project Options.1784.png
  4. Select [Yes] when asked to Open Associated Perspective.1785.png

After this is done, the device configuration tool view is open in STM32CubeIDE. From here on, we can configure the MCU to be able to utilize the board's SD card slot.

2. SDMMC configuration

STM32 MCUs use the SDMMC peripheral to interface to an SD card, we need to configure it before we can write code that uses it. In this article, we also configure DMA access to the SDMMC peripheral to maximize performance.

  1. In the Device Configuration Tool view, for the “SDMMC1” peripheral, which is located in the “Connectivity” category, set the "Mode" parameter to "SD 4 bits Wide bus".1786.png
  2. In the DMA Settings panel, add DMA requests for SDMMC1_TX and SDMMC1_RX with their default settings.pepfof_0-1755095525756.png
     
     
     
     

    After adding these requests, the DMA settings panel should look like this:

    pepfof_1-1755095631544.png

3. FatFs configuration

FatFs is an open-source file system middleware integrated in STM32Cube libraries. It is able to directly utilize the SDMMC peripheral to act as a disk device for the FAT file system. This is also configured through the Device Configuration Tool view.

  1. In the "Middleware" category, for the FATFS middleware, enable the "SD card" option. In the "Platform Settings" panel, select "PC13 [uSD_Detect]" as a solution for "Detect_SDIO".1788.png
  2. As we are using DMA to access the SDMMC peripheral, in the "Advanced Settings" panel, enable the "Use dma template" option.pepfof_3-1755096797869.png

     

4. Project Configuration and code generation

After the peripheral and middleware configuration is complete, we will also need to modify the clock configuration and certain project settings.

  1. The default clock configuration for this MCU presents an issue with the clock input to the SDMMC controller. This needs to be resolved, and can be done easily by going to the "Clock Configuration" tab and selecting [Yes] when asked to automatically resolve clock issues.1790.png
  2. Lastly, the FatFs middleware requires additional memory for the Heap and the Stack. In the Project Manager tab, set the "Minimum Heap Size" and "Minimum Stack Size" parameters for the Linker Settings to "0x400" and "0x800" respectively.1791.png
  3. When you save the project, the IDE presents you with an option to generate code according to your Device Configuration Tool setup. Select [Yes] when asked to generate the code.1792.png
  4. Select [Yes] when asked to Open Associated Perspective. This will take you to your project's generated main source file.1793.png

5. Create a demo application

Now that SDMMC and FatFs configuration is complete and the appropriate code is generated, we can start writing user code that accesses the SD card. For the purposes of this article, the code sample below mounts the SD card, create a new FAT file system on it, create a file named "STM32.TXT", and write "STM32 FATFS works great!" to it.

You may copy this snippet into your main.c file - take note of the "/* USER CODE BEGIN x */" markers and place the two sections in the places that these are located in your code.

/* USER CODE BEGIN 1 */
FRESULT res; /* FatFs function common result code */
uint32_t byteswritten, bytesread; /* File write/read counts */
uint8_t wtext[] = "STM32 FATFS works great!"; /* File write buffer */
uint8_t rtext[_MAX_SS];/* File read buffer */
/* USER CODE END 1 */
 ...
/* USER CODE BEGIN 2 */
	if(f_mount(&SDFatFS, (TCHAR const*)SDPath, 0) != FR_OK)
	{
		Error_Handler();
	}
	else
	{
		if(f_mkfs((TCHAR const*)SDPath, FM_ANY, 0, rtext, sizeof(rtext)) != FR_OK)
	 {
			Error_Handler();
	 }
		else
		{
			//Open file for writing (Create)
			if(f_open(&SDFile, "STM32.TXT", FA_CREATE_ALWAYS | FA_WRITE) != FR_OK)
			{
				Error_Handler();
			}
			else
			{

				//Write to the text file
				res = f_write(&SDFile, wtext, strlen((char *)wtext), (void *)&byteswritten);
				if((byteswritten == 0) || (res != FR_OK))
				{
					Error_Handler();
				}
				else
				{

					f_close(&SDFile);
				}
			}
		}
	}
	f_mount(&SDFatFS, (TCHAR const*)NULL, 0);
/* USER CODE END 2 */

6. Build and flash the code

Finally, you may build the project and run it on the device by starting a debug session.

1794.png
pepfof_0-1755098006776.pngWhen the code is executed, the SD card is formatted and the text file is written to it. Inserting the SD card into a host PC, you may read the file, as presented in the screenshot to the right.

 


 

Related links

 

 

Video

 

This topic has been closed for replies.

16 replies

rwils.1
Associate III
Jul 26, 2022 6:27 PM UTC

Has anyone tried this code on a STM32L471RGT6? It doesn't appear to work and fails at line if(f_mkfs((TCHAR const*)SDPath, FM_ANY, 0, rtext, sizeof(rtext)) != FR_OK

Thanks in advance

DWils.3
Visitor II
Oct 1, 2022 3:03 PM UTC

I'm using a different board and connector. My connector's detect switch is active high. I had to change this line of code in fatfs_platform.c from "RESET" to "SET".

if(HAL_GPIO_ReadPin(SD_DETECT_GPIO_PORT, SD_DETECT_PIN) != GPIO_PIN_SET)

This has to be changed to set anytime the ioc file is updated.

Also, try setting the SDMMC clock divide factor to something greater than 0. 0x80 for example. ioc configuration, SDMMC1, Parameters tab.

TKana.1
Associate III
Feb 1, 2023 3:30 PM UTC

Hi,

I am using the same dev board. Followed all the steps above. My STCubeIDE version is 1.11.2. Program gets stuck at:

if(f_mkfs((TCHAR const*)SDPath, FM_ANY, 0, rtext, sizeof(rtext)) != FR_OK)

{

Error_Handler();

}

with "FR_NOT_READY"

checked and rechecked again, used various SDCards but same.

Any advice is appreciated.

Thanks,

Tim

TKana.1
Associate III
Feb 3, 2023 6:43 AM UTC

Made it work with couple of modifications:

1- Moved variables to global

move

"

/* USER CODE BEGIN 1 */

FRESULT res; /* FatFs function common result code */

uint32_t byteswritten, bytesread; /* File write/read counts */

uint8_t wtext[] = "STM32 FATFS works great!"; /* File write buffer */

uint8_t rtext[_MAX_SS];/* File read buffer */

/* USER CODE END 1 */

"

to

"

* USER CODE BEGIN PV */

FRESULT res; /* FatFs function common result code */

uint32_t byteswritten, bytesread; /* File write/read counts */

uint8_t wtext[] = "STM32 FATFS cali666siy great!"; /* File write buffer */

uint8_t rtext[_MAX_SS];/* File read buffer */

/* USER CODE END PV */

"

2- Changed 4B wide operation to 1B operation in "MX_SDMMC1_SD_Init()"

static void MX_SDMMC1_SD_Init(void)

{

 /* USER CODE BEGIN SDMMC1_Init 0 */

 /* USER CODE END SDMMC1_Init 0 */

 /* USER CODE BEGIN SDMMC1_Init 1 */

 /* USER CODE END SDMMC1_Init 1 */

 hsd1.Instance = SDMMC1;

 hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;

 hsd1.Init.ClockBypass = SDMMC_CLOCK_BYPASS_DISABLE;

 hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;

 hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B; //Start with 1B instead 4B. Later "SD_Widebus_Enable" command makes it 4B

 hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;

 hsd1.Init.ClockDiv = 0;

 /* USER CODE BEGIN SDMMC1_Init 2 */

 /* USER CODE END SDMMC1_Init 2 */

}

now it works OK. Tested with 4GB and 16GB FAT32 formatted uSD cards

Tim

Visitor II
Apr 29, 2023 8:48 PM UTC

Thank's for your advice, now my SD Card program works fine.

Associate II
Jun 26, 2023 5:50 AM UTC

My code does not work, I even moved some variables to global, still not working. Please help me out. My hardware PCB uses a 4-bit wide bus, and my SD Card is FAT32 8GB. It only works upto f_mount() which returns FR_OK, but after that, the f_open returns FR_DISK_ERR.

Stanys.1
Associate
Nov 13, 2023 4:34 PM UTC

I had the same problem with f_mount(). I use the same solution as described by JBond.1

https://community.st.com/t5/stm32cubemx-mcus/sdcard-does-not-work-with-4bits-wide-bus/td-p/602607

It works fine! You don't need to do the steps described by TKana.1

I use STM32CubeIDE Version: 1.13.2 and STM32CubeF4 Firmware Package V1.27.0 / 11-February-2022

Associate II
Jan 9, 2024 6:19 AM UTC

Hello, Can anyone Tell me is it mandatory to Format a new SD Card before writing or Reading data in STM32 MCU. Currently I am facing an issue wherein whenever I try to write data into a new non-formatted SD Card, It gives me an error but whenever I try to write data into a SD card using a card reader, it gets written. Thanks for help in advance.

AScha.3
Super User
Jan 9, 2024 6:43 AM UTC

Hi,

>is it mandatory to Format a new SD Card

NO!  You should never format a new sd-card, because they are format to the optimum for that card.

So format -especially as first action on a new system- might with good chance destroy the card or at least make it worse (getting slower) . Especially on new, big (> 32GB) cards in exfat format.

Also dont write - until mount, open directory and reading files working perfect.  Then can try write something.

If you feel a post has answered your question, please click on " Best Answer ".
Associate III
Jan 23, 2024 2:55 PM UTC

Like others it failed at f_mkfs.  I watched the video for this guide...

https://www.youtube.com/watch?v=I9KDN1o6924 

...and there is a step missing from this written guide.  The missing step, as shown in the video, is to add the DMA Rx and Tx..

johngj_0-1706021484303.png

Since adding the dma rx/tx and changing the SD mode from 4 bit wide to 1 bit, it now works.

For some reason it does not work in SD mode 4 bit wide