cancel
Showing results for 
Search instead for 
Did you mean: 

Update a wildcard in a custom container called in a scroll wheel

Roombr_VI
Associate II

In my main screen there is a scroll wheel which scrolls the contents of a custom container. The custom container has 5 wildcards. Now I intend to dynamically update those wildcards with my text resources. But I'm unable to do so. Please find my codes attached.

 

Screen1View.cpp

 

#include <gui/screen1_screen/Screen1View.hpp>
#include <texts/TextKeysAndLanguages.hpp>



void TextUpdate::updateText()
{
	Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%s", touchgfx::TypedText(T_NAT_EVE1).getText());
	    textArea1.setWildcard(textArea1Buffer);
	    textArea1.setTypedText(touchgfx::TypedText(T_NAT_EVE1));
	    add(textArea1);
}

// Screen1View constructor
Screen1View::Screen1View()
    : tickCounter(0), targetItem(0), scrollCompleted(false),
      digitalHours(0), digitalMinutes(0), digitalSeconds(0),
      textUpdateIntervalCounter(0), textUpdateObj() // Initialize textUpdateObj
{
}

void Screen1View::setupScreen()
{
    Screen1ViewBase::setupScreen();

    tickCounter = 0;  // Reset the tick counter
    textUpdateIntervalCounter = 0; // Reset the interval counter
    targetItem = scrollWheel1.getSelectedItem(); // Initialize target item
    scrollCompleted = false; // Reset scroll completion flag
    digitalHours = digitalClock1.getCurrentHour();
    digitalMinutes = digitalClock1.getCurrentMinute();
    digitalSeconds = digitalClock1.getCurrentSecond();
}

void Screen1View::tearDownScreen()
{
    Screen1ViewBase::tearDownScreen();
}

void Screen1View::handleTickEvent()
{
    tickCounter++;
    textUpdateIntervalCounter++;

    // Scroll logic: Execute every 0.5 seconds (30 ticks at 60 Hz)
    if (tickCounter % ticksPerStep == 0)
    {
        if (!scrollWheel1.isAnimating() && !scrollCompleted)
        {
            targetItem = (targetItem + 1) % scrollWheel1.getNumberOfItems();
            scrollWheel1.animateToItem(targetItem, 500); // Smooth animation (500ms)
            scrollCompleted = true;
        }
        else if (!scrollWheel1.isAnimating() && scrollCompleted)
        {
            scrollCompleted = false; // Reset flag when animation finishes
        }
    }

    // Clock update logic: Execute every second
    if (tickCounter % 60 == 0)
    {
    	textUpdateObj.updateText();
        if (++digitalSeconds >= 60)
        {
            digitalSeconds = 0;
            if (++digitalMinutes >= 60)
            {
                digitalMinutes = 0;
                if (++digitalHours >= 24)
                {
                    digitalHours = 0;
                }
            }
        }

        digitalClock1.setTime24Hour(digitalHours, digitalMinutes, digitalSeconds);
    }

    // Text update logic: Execute every 2 seconds (120 ticks at 60 Hz)
    if (textUpdateIntervalCounter >= 120)
    {
    	        textUpdateObj.updateText(); // Update text dynamically
    	        textUpdateIntervalCounter = 0;
    }
}

void Screen1View::resetScroll()
{
    tickCounter = 0;            // Reset tick counter
    scrollCompleted = false;    // Allow scrolling again
}

 

 

 

 Screen1View.hpp

 

#ifndef SCREEN1VIEW_HPP
#define SCREEN1VIEW_HPP

#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
#include <gui_generated/containers/CustomContainer1Base.hpp>

class TextUpdate : public CustomContainer1Base
{
public:
   // TextUpdate();
    //virtual ~TextUpdate(){}
    virtual void updateText();
};

class Screen1View : public Screen1ViewBase
{
public:
    Screen1View();
    virtual ~Screen1View() {}

    virtual void setupScreen();
    virtual void tearDownScreen();
    virtual void handleTickEvent();

    void resetScroll(); // Method to reset the scroll state

protected:
    int tickCounter;        // Counter to track ticks
    int targetItem;         // The target index for the scroll wheel
    bool scrollCompleted;   // Flag to ensure the scroll happens only once
    static constexpr int ticksPerStep = 30; // Number of ticks for a 0.5-second delay (assuming 60 Hz)
    int digitalHours;
    int digitalMinutes;
    int digitalSeconds;

    int textUpdateIntervalCounter; // Counter for updating text every 2 seconds
    TextUpdate textUpdateObj;      // Object for TextUpdate
};

#endif // SCREEN1VIEW_HPP

 

 

 

I intend to print only in the first wildcard for the time being.

13 REPLIES 13
MM..1
Chief III
add(textArea1);

This update text on other paralel universum... try

textArea1.invalidate();

 

I did try,

textArea1.invalidate();

But it still does not update any wildcards

void TextUpdate::updateText()
{
	Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%s", touchgfx::TypedText(T_NAT_EVE1).getText());
	    textArea1.setWildcard(textArea1Buffer);
	    textArea1.setTypedText(touchgfx::TypedText(T_NAT_EVE1));

you update nothink then you nothink change see...

Roombr_VI
Associate II

I have tried both these variations

void TextUpdate::updateText()
{
	Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%s", touchgfx::TypedText(T_NAT_EVE1).getText());
	    textArea1.setWildcard(textArea1Buffer);
	    textArea1.setTypedText(touchgfx::TypedText(T_NAT_EVE1));
	    add(textArea1);
	    textArea1.invalidate();
}

and 

void TextUpdate::updateText()
{
	Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%s", touchgfx::TypedText(T_NAT_EVE1).getText());
	    textArea1.setWildcard(textArea1Buffer);
	    textArea1.setTypedText(touchgfx::TypedText(T_NAT_EVE1));
	    textArea1.invalidate();
}

Have you basic C++ knowledge?? Your try work with containers is complete wrong.

ferro
Senior III

Hi @Roombr_VI 

Please share an example project with the code in your question.

GaetanGodart
ST Employee

Hello @Roombr_VI ,

 

Sharing your whole project (as a 7z file) would help us understand what you want to achieve.

The scrollWhell uses callbacks to update its elements (the custom containers that are inside the scrollWheel).
There are 2 native callbacks :

You read the API documentation for the scrollWheel here .

Also, to setup these callbacks, I invite you to watch this video  (on 75% or 50% speed maybe).

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Please find the compressed file below. I'm trying to update the wildcard in the scroll wheel with the text resources. I'm quite new to C++ so I may have made a few errors. 

"I'm quite new to C++ so I may have made a few errors. "

The code does not build. Please fix it.

\Digital_scroll\TouchGFX\gui\src\screen1_screen\Screen1View.cpp(9,55): error C2039: 'scrollWheel11AnimateToHandler': is not a member of 'Screen1View