cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFXDesigner cannot run target

rhine1012
Associate II

1. Developing tools directories as this:

D:\ProgramData\STMicroelectronics\STM32Cube\STM32CubeMX
D:\ProgramData\STMicroelectronics\STM32Cube\STM32CubeProgrammer
D:\ProgramData\STMicroelectronics\TouchGFX\4.24.2\

2. ST link drivers are installed well.(because code can be compiled and downloaded via usb ST-link)

3. Hardware is STM32U5A9J-DK.

4. TouchGFX Designer demo is TouchGFX Demo6. Run simulator is OK.

demo6.PNG

target.PNG

 My question is:

   I want to run this demo on STM32U5A9J-DK, but the run button can not work and display 'Cannot Run Target'.

   which procedure is wrong? Or is there any guidance to solve this problem?

 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Did you select first the board STM32U5A9J-DK in the Board setup before creating the demo?

SofLit_0-1738774339949.png

SofLit_1-1738774394632.png

SofLit_2-1738774454755.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
mƎALLEm
ST Employee

Hello,

Did you select first the board STM32U5A9J-DK in the Board setup before creating the demo?

SofLit_0-1738774339949.png

SofLit_1-1738774394632.png

SofLit_2-1738774454755.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

It works,thank you!