2025-02-05 8:48 AM
1. Developing tools directories as this:
D:\ProgramData\STMicroelectronics\STM32Cube\STM32CubeMX
D:\ProgramData\STMicroelectronics\STM32Cube\STM32CubeProgrammer
D:\ProgramData\STMicroelectronics\TouchGFX\4.24.2\
2. ST link drivers are installed well.(because code can be compiled and downloaded via usb ST-link)
3. Hardware is STM32U5A9J-DK.
4. TouchGFX Designer demo is TouchGFX Demo6. Run simulator is OK.
My question is:
I want to run this demo on STM32U5A9J-DK, but the run button can not work and display 'Cannot Run Target'.
which procedure is wrong? Or is there any guidance to solve this problem?
Solved! Go to Solution.
2025-02-05 8:53 AM - edited 2025-02-05 8:54 AM
Hello,
Did you select first the board STM32U5A9J-DK in the Board setup before creating the demo?
2025-02-05 8:53 AM - edited 2025-02-05 8:54 AM
Hello,
Did you select first the board STM32U5A9J-DK in the Board setup before creating the demo?
2025-02-06 8:14 AM
It works,thank you!