2020-02-17 6:57 AM
All declarations in the global namespace that start with an underscore are reserved by the C++ compiler according to the C++ standard. See: https://en.cppreference.com/w/cpp/keyword
TouchGFX violates this by converting any images to "_filename" and having them in the global namespace. I was made aware of this when an image with the name "start" was colliding with the compiler's defined value of _start.
This should be fixed as soon as possible.
Solved! Go to Solution.
2020-02-18 5:11 AM
Hi @j o,
You're right. If an image asset starts with an upper-case letter, the resulting symbol is reserved according to the c++ standard. It's never been an issue for us or anyone else (that i know of), but there's a task in our system to fix this in the image converter tool.
So, you could say that TouchGFX allows the user to violate the standard, depending on how assets are named, yes.
Thanks for highlighting it =)
/Martin
2020-02-18 5:11 AM
Hi @j o,
You're right. If an image asset starts with an upper-case letter, the resulting symbol is reserved according to the c++ standard. It's never been an issue for us or anyone else (that i know of), but there's a task in our system to fix this in the image converter tool.
So, you could say that TouchGFX allows the user to violate the standard, depending on how assets are named, yes.
Thanks for highlighting it =)
/Martin
2020-02-18 5:25 AM
Hi Martin,
I'd like to clarify, that *in the global namespace* (which this is) any leading underscores whether they are followed by upper-case or not, are in violation. The leading underscore can't be used *anywhere* if a capital letter follows. See the following quote from the linked site (emphasis mine):
"Also, all identifiers that contain a double underscore __ in any position and each identifier that begins with an underscore followed by an uppercase letter is always reserved and all identifiers that begin with an underscore are reserved for use as names in the global namespace. See identifiers for more details."
Regards,
Jeremy
2020-02-18 5:44 AM
I think we'll prioritize this since it's a quick fix, tests pending. Will bundle it as a "tool patch" with a fix to the fontconverter that's already in the "known issues".