2021-08-14 6:56 AM
I am using TouchGfx 4.17 together with stm32cubeide 1.7.0.
Right at the moment I'm trying out all the TouchGfx tutorials.
I really like all the word- and code completion-, content assist. and parameter hints features of stm32cubeIDE, but it seems that none of these features work in a TouchGfx-Designer-generated project any more.
I can't find the right setting in stm32CubeIDE for enabling those features; it seems that they are already enabled but somehow refuse to work.
So, what settings in stm32cubeIDE should I change so that all the nice features that work perfectly with the HAL library also work with TouchGfx?
2021-08-18 9:38 PM
Hello CRaus.1,
I added STM32CubeIDE as a topic because this is not directly linked to TouchGFX.
/Alexandre
2021-09-09 1:32 AM
Hi,
Were you able to find how to enable those features ? Seems interesting.
/Romain