cancel
Showing results for 
Search instead for 
Did you mean: 

touchgfx + stm32cubeide: how to enable word- and code completion, content assist, parameter hints?

papamidas
Associate II

I am using TouchGfx 4.17 together with stm32cubeide 1.7.0.

Right at the moment I'm trying out all the TouchGfx tutorials.

I really like all the word- and code completion-, content assist. and parameter hints features of stm32cubeIDE, but it seems that none of these features work in a TouchGfx-Designer-generated project any more.

I can't find the right setting in stm32CubeIDE for enabling those features; it seems that they are already enabled but somehow refuse to work.

So, what settings in stm32cubeIDE should I change so that all the nice features that work perfectly with the HAL library also work with TouchGfx? 

2 REPLIES 2
Alexandre RENOUX
Principal

Hello CRaus.1,

I added STM32CubeIDE as a topic because this is not directly linked to TouchGFX.

/Alexandre

Romain DIELEMAN
ST Employee

Hi,

Were you able to find how to enable those features ? Seems interesting.

/Romain