2020-09-10 11:50 PM
안녕하세요.
Modal�?� �?�운 �?태�?서 터치스�?�린 입력�?� 받아서 사�?�지게 하고 싶습니다.
버튼 키를 사용하지 않고 스�?�린 아무곳�?� 터치 해�?� 받�?�수 있는 방법�?� 있나요?
답변 부�?드리겠습니다.
�?사 합니다.
2020-09-11 12:22 AM
해결 했습니다.
2020-09-11 01:18 AM
Hello @Phyo .1 ,
Please try to write in English because most of the people on this community can speak English but not Korean.
I used Google translate to get an rough idea of what you are saying but may be it's unclear.
Then, please share the way that solved your problem, it may be helpful for other community users.
Thank you for your contribution.
Here is your message using Google translate:
"Can I get keys from TouchGFX Modal?
Hello,
I want to make it disappear by receiving a touch screen input while the modal is open.
Is there a way to get it by touching anywhere on the screen without using the button keys?
Please answer.
Thank you.
I solved it.
"
Best Regards,
imen
2020-09-11 05:00 AM
Hello @Phyo .1
Have you looked at the Modal Window example available in TouchGFX Designer ?
Because it implements a button inside the modal window that is clickable by TouchEvent.
/Alexandre