2023-03-31 12:00 AM
last time also this problem was occured so I installed it again after that it run for some days now again the problem has occured.
When I open Touchgfx one msg come
Sorry - something unexpected has happened which caused an error to occur in the Designer.
For more information, see the log file located at: C:\Users\Kaushal\AppData\Roaming\TouchGFX-4.21.3\TouchGFXDesigner.log
Please someone help to give the solution of it.
Solved! Go to Solution.
2023-05-08 6:43 AM - edited 2023-11-20 9:05 AM
Hello @MPath.4,
You can manually install the generator, by following the steps described at the bottom of this post.
/Yoann
2023-03-31 1:08 AM
Hello @MPath.4,
When does that happen? Right after launching TouchGFXDesigner? Or after doing something specific while designing your application?
Could you also share the log file you referred to?
Thank you.
/Yoann
2023-03-31 1:43 AM
2023-03-31 1:45 AM
2023-03-31 9:18 PM
Last day I made one application and closed it after that and the next day I opened but it had given the error.
2023-04-03 12:39 AM
Hello,
Could you share the whole .log file ? Would be better for debugging.
Thanks,
/Yoann
2023-04-04 10:50 PM
2023-04-04 11:18 PM
Still it's not opening
2023-04-10 10:39 PM
I download the version 4.20.0 of Touchgfx designer and it's working then why the version 4.21.3 is not working.
2023-04-11 8:14 AM
Hello,
I discussed your issue with my colleagues and we think that it could come from something written under a wrong format inside the .touchgfx file of your project.
Could you please share it here so we can check that ?
Thanks
/Yoann