cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX demo screen is not working properly on STM32429I-EVAL1

ESKim
Associate

Hello,

I'm going to run demo by referring to the TouchGFX Documentation.​

But, When I run target after code generating in TouchGFX Designer, the screen does not ​display properly. Did I make a mistake? The same problem occurs again and again.

Board: STM32429I-EVAL1

TouchGFX Version: 4.20.0​

STM32CubeMX Version: 6.6.1

STM32CubeIDE Version: 1.10.1

STM32CubeProgrammer Version: 2.11.0

0693W00000WJPN6QAP.jpg0693W00000WJPJiQAP.jpg

Thank you in advance for your response.

2 REPLIES 2
MM..1
Chief II

In designer on left click Config and locate Image default angle. Change 0 to 90 .

Romain DIELEMAN
ST Employee

From your picture and how the images look I suppose the external loader has not been selected. Try to use STM32CubeProgrammer to launch your project and select the right external loader (do you know how to do that ? We can share the steps if not). This is odd that you would face this if you are using a project started from TouchGFX Designer with the TouchGFX Board Setup for the STM32429I-EVAL1.

/Romain