cancel
Showing results for 
Search instead for 
Did you mean: 

Touchgfx 4.17.0's project with one button returns [ExtFlashSection]: No space left on device

Zu
Associate II

Hello,

I think something is broken with the last release of touchgfx or something shady is missing in my setup.

my setup:

Touchgfx 4.17.0

Stm board: STM32H735G-DK touchgfx VERSION V 3.0.4

Stm32Cube FW: 1.9.0 Drivers

Steps:

  • Make a new project
  • put a box and a button In the middle of the screen
  • generate code
  • run on target

I get this error on the console

Run Target
    Generate
        Done
    Generate Assets
        make -f simulator/gcc/Makefile assets -j8
        Reading ./application.config
        Done
    Post Generate
        touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
        Done
    Post Generate Target
        touchgfx update_project --project-file=../STM32H735G-DK.ioc --platform=m7
        .project files generated inside project folder
        This is STM32CubeIDE project updater: Working on ../STM32CubeIDE/.project
        Project file: ../STM32CubeIDE/.cproject
        Done
    Compile
        make -f ../gcc/Makefile -j8
        Reading TouchGFX/application.config
        Linking TouchGFX/build/bin/target.elf
        Producing additional output formats...
          target.hex   - Combined internal+external hex
          intflash.elf - Internal flash, elf debug
          intflash.hex - Internal flash, hex
          extflash.bin - External flash, binary
        C:\TouchGFX\4.17.0\env\MinGW\msys\1.0\gnu-arm-gcc\bin\arm-none-eabi-objcopy.exe:TouchGFX/build/bin/extflash.bin[ExtFlashSection]: No space left on device
        gcc/Makefile:286: recipe for target 'TouchGFX/build/bin/target.elf' failed
        make[2]: *** [TouchGFX/build/bin/target.elf] Error 1
        gcc/Makefile:282: recipe for target 'generate_assets' failed
        make[1]: *** [generate_assets] Error 2
        ../gcc/Makefile:49: recipe for target 'all' failed
        make: *** [all] Error 2
        Failed
    Failed

If I open any other project made with Touchgfx 4.16.x it works without any problem.

I attached here the generated project

3 REPLIES 3
MM..1
Chief III

How free space on HDD you have for this project... Extflash.bin is ugly big file...

Zu
Associate II

20gb available

filesystem that support bigger files as 2G ?