2021-05-19 12:47 AM
When I generate code on my TouchFGX 4.15.0 project, it overwrites the correct Library Search Path in my STM32CubeIDE .cproject file and replaces it with this one:
"${workspace_loc:/Executable/Middlewares/ST/TouchGFX/touchgfx/lib/core/cortex_m7/gcc}}"
In fact the correct location for the library is:
"${workspace_loc:/${ProjName}/Middlewares/ST/TouchGFX/touchgfx/lib/core/cortex_m7/gcc}"
I can't find any way to change this in the .touchgfx file or elsewhere. How can I correct this so I don't need to manually change every time I regenerate the code?
2021-05-26 6:15 PM
Anyone? @Martin KJELDSEN can you help with this?
2021-05-27 12:14 AM
Hi,
Do you also face this issue with TouchGFX 4.16.1 ? How did you create your project ? Was it from scratch or did you use an application template for one of ST development kits ?
/Romain
2021-05-27 12:21 AM
Hi,
I haven't tried with 4.16.1, still running 4.15. I originally created my project when TouchGFX was first introduced into CubeMX - I think TouchGFX Version 4.10 or similar. I used the code generator to create the project. It started to behave badly after migrating to V4.15.
2021-05-27 3:13 AM
Hi. Pretty sure we fixed something like that in the following releases. It's not a configuration you'll find in the .project file. It happens during post-generation to include all the right files in your projects.
I could point you to the ruby scripts that modify this path inside the installed TouchGFX Environment if you want to have a look. Maybe we'll provide a patch for you.
/Martin