cancel
Showing results for 
Search instead for 
Did you mean: 

TextArea value: the simulation does not match the reality

FTrom
Associate II

Hi

I am new in the touchGFX, so I think/hope that I did a silly error.

By the simulation i could simply change the a float value shown in a TextArea using a bar progress or buttons.

From the simulation all works properly, but when I flash the software in the STM32750Disckovery kit, I can see "-in" instead of the value.

Attached the flles of the screen.

Thanks

1712837437331.jpg

 

3 REPLIES 3
GaetanGodart
ST Employee

Hello @FTrom ,

 

In your post you say you attached some files but I do not see any (it could be beneficial to have the whole project in a zip rather than just the view.cpp file).

Could you also share a screenshot of the proper expected behavior (simulator).

Which version of TouchGFX are you using?

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)
MM..1
Chief II
GaetanGodart
ST Employee

Hello @FTrom ,

 

Were you able to move forward with your project?

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)