2020-12-01 8:51 AM
Hello,
I am developing on STM32L4R9I-Disco, and I want to display ARGB8888 images on the round DSI display under the command of UART. For example, I send hex 'b2' to this board by uart, one image is displayed.
I have succeeded some parts, but the image is not well displayed (the attached picture).
Anyone knows what's the problem?
Thank you.
Here are some parts of the program:
#define VSYNC 1
#define VBP 1
#define VFP 1
#define VACT 390
#define HSYNC 1
#define HBP 1
#define HFP 1
#define HACT 390
#define LAYER_ADDRESS GFXMMU_VIRTUAL_BUFFER0_BASE
static void CopyInVirtualBuffer_single(uint32_t *pSrc,
uint32_t *pDst,
uint16_t xsize,
uint16_t ysize);
UART part:
uint8_t Rx_data[10];
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
HAL_UART_Receive_IT(&huart2, Rx_data, 1);
if (Rx_data[0] == 0xb2)
{
CopyInVirtualBuffer_single((uint32_t*) image_img_01_ARGB, (uint32_t*) LAYER_ADDRESS, 390, 390);
pending_buffer = 1;
HAL_DSI_Refresh(&DsiHandle);
HAL_GPIO_TogglePin(GPIOH, GPIO_PIN_4);
}
}
main:
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_USART3_UART_Init();
HAL_UART_Receive_IT(&huart2, Rx_data, 1);
BSP_LED_Init(LED1);
BSP_LED_Init(LED2);
if(LCD_Config() != LCD_OK)
{
Error_Handler();
}
while (1)
{
}
some configurations:
__HAL_GFXMMU_RESET_HANDLE_STATE(&GfxmmuHandle);
GfxmmuHandle.Instance = GFXMMU;
GfxmmuHandle.Init.BlocksPerLine = GFXMMU_192BLOCKS;
GfxmmuHandle.Init.DefaultValue = 0xFFFFFFFF;
GfxmmuHandle.Init.Buffers.Buf0Address = (uint32_t) PhysFrameBuffer;
GfxmmuHandle.Init.Buffers.Buf1Address = 0; /* Not Used */
GfxmmuHandle.Init.Buffers.Buf2Address = 0; /* Not Used */
GfxmmuHandle.Init.Buffers.Buf3Address = 0; /* Not Used */
GfxmmuHandle.Init.Interrupts.Activation = ENABLE; //DISABLE
//GfxmmuHandle.Init.Interrupts.UsedInterrupts = GFXMMU_AHB_MASTER_ERROR_IT; /* Not Used */
if(HAL_OK != HAL_GFXMMU_Init(&GfxmmuHandle))
{
return(LCD_ERROR);
}
if(HAL_OK != HAL_GFXMMU_ConfigLut(&GfxmmuHandle, 0, 390, (uint32_t) gfxmmu_lut_config_32))
{
return(LCD_ERROR);
}
if(HAL_OK != HAL_GFXMMU_DisableLutLines(&GfxmmuHandle, 390, 634))
{
return(LCD_ERROR);
}
__HAL_LTDC_RESET_HANDLE_STATE(&LtdcHandle);
LtdcHandle.Instance = LTDC;
LtdcHandle.Init.HSPolarity = LTDC_HSPOLARITY_AL;
LtdcHandle.Init.VSPolarity = LTDC_VSPOLARITY_AL;
LtdcHandle.Init.DEPolarity = LTDC_DEPOLARITY_AL;
LtdcHandle.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
LtdcHandle.Init.HorizontalSync = 0; /* HSYNC width - 1 */
LtdcHandle.Init.VerticalSync = 0; /* VSYNC width - 1 */
LtdcHandle.Init.AccumulatedHBP = 1; /* HSYNC width + HBP - 1 */
LtdcHandle.Init.AccumulatedVBP = 1; /* VSYNC width + VBP - 1 */
LtdcHandle.Init.AccumulatedActiveW = 391; /* HSYNC width + HBP + Active width - 1 */
LtdcHandle.Init.AccumulatedActiveH = 391; /* VSYNC width + VBP + Active height - 1 */
LtdcHandle.Init.TotalWidth = 392; /* HSYNC width + HBP + Active width + HFP - 1 */
LtdcHandle.Init.TotalHeigh = 392; /* VSYNC width + VBP + Active height + VFP - 1 */
LtdcHandle.Init.Backcolor.Red = 0; /* Not used default value */
LtdcHandle.Init.Backcolor.Green = 0; /* Not used default value */
LtdcHandle.Init.Backcolor.Blue = 0; /* Not used default value */
LtdcHandle.Init.Backcolor.Reserved = 0xFF;
if(HAL_LTDC_Init(&LtdcHandle) != HAL_OK)
{
return(LCD_ERROR);
}
/* LTDC layer 1 configuration */
LayerCfg.WindowX0 = 0;
LayerCfg.WindowX1 = 390;
LayerCfg.WindowY0 = 0;
LayerCfg.WindowY1 = 390;
//LayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB888;
//LayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_ARGB1555;
LayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_ARGB8888;
LayerCfg.Alpha = 0xFF; /* NU default value */
LayerCfg.Alpha0 = 0; /* NU default value */
LayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_PAxCA; /* Not Used: default value */
LayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_PAxCA; /* Not Used: default value */
LayerCfg.FBStartAdress = LAYER_ADDRESS;
LayerCfg.ImageWidth = 390;
LayerCfg.ImageHeight = 390;
LayerCfg.Backcolor.Red = 0; /* Not Used: default value */
LayerCfg.Backcolor.Green = 0; /* Not Used: default value */
LayerCfg.Backcolor.Blue = 0; /* Not Used: default value */
LayerCfg.Backcolor.Reserved = 0xFF;
if(HAL_LTDC_ConfigLayer(&LtdcHandle, &LayerCfg, 0) != HAL_OK) //LTDC_LAYER_1 --> 0
{
return(LCD_ERROR);
}
if (HAL_LTDC_SetPitch(&LtdcHandle, 768, 0) != HAL_OK)
{
return(LCD_ERROR);
}
static void CopyInVirtualBuffer_single(uint32_t *pSrc, uint32_t *pDst, uint16_t xsize, uint16_t ysize)
{
uint32_t source = (uint32_t)pSrc;
Dma2dHandle.Instance = DMA2D;
/*##-1- Configure the DMA2D Mode, Color Mode and output offset #############*/
Dma2dHandle.Init.Mode = DMA2D_M2M;
Dma2dHandle.Init.ColorMode = DMA2D_OUTPUT_ARGB8888;
Dma2dHandle.Init.OutputOffset = 768 - xsize;
Dma2dHandle.Init.AlphaInverted = DMA2D_REGULAR_ALPHA; /* No Output Alpha Inversion */
Dma2dHandle.Init.RedBlueSwap = DMA2D_RB_REGULAR; /* No Output Red & Blue swap */
Dma2dHandle.Init.BytesSwap = DMA2D_BYTES_REGULAR; /* Regular output byte order */
Dma2dHandle.Init.LineOffsetMode = DMA2D_LOM_PIXELS; /* Pixel mode */
/*##-2- Foreground Configuration ###########################################*/
Dma2dHandle.LayerCfg[1].InputColorMode = DMA2D_INPUT_ARGB8888;
Dma2dHandle.LayerCfg[1].InputOffset = 0;
Dma2dHandle.LayerCfg[1].AlphaMode = DMA2D_NO_MODIF_ALPHA;
Dma2dHandle.LayerCfg[1].InputAlpha = 0xFF; /* Not used */
Dma2dHandle.LayerCfg[1].RedBlueSwap = DMA2D_RB_SWAP; //DMA2D_RB_REGULAR; /* No ForeGround Red/Blue swap */
Dma2dHandle.LayerCfg[1].AlphaInverted = DMA2D_REGULAR_ALPHA; /* No ForeGround Alpha inversion */
/* DMA2D Initialization */
if(HAL_DMA2D_Init(&Dma2dHandle) == HAL_OK)
{
if(HAL_DMA2D_ConfigLayer(&Dma2dHandle, 1) == HAL_OK)
{
if (HAL_DMA2D_Start(&Dma2dHandle, source, LAYER_ADDRESS, xsize, ysize) == HAL_OK)
{
/* Polling For DMA transfer */
HAL_DMA2D_PollForTransfer(&Dma2dHandle, 10);
}
}
}
}
Solved! Go to Solution.
2020-12-04 3:57 AM
Here is the solution: define the output of DAM2D as RGB888 or RGB565, not ARGB8888.
2020-12-01 10:41 AM
??? how is your problem ??? why 768-xsize offset
2020-12-02 1:42 AM
The image is tore into 2 parts, and it is inverted (the black in the photo)
768 - xsize: I use GFXMMU, it is the same with the example DSI_CmdMode_SingleBuffer in the firmware package.
Line offset = virtual buffer line width in pixels - image width in pixels.
2020-12-04 3:57 AM
Here is the solution: define the output of DAM2D as RGB888 or RGB565, not ARGB8888.