cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7BWorkshop2020, I upgrade IDE, TouchGFX, Firmware repository to 1.08 and all. Started from fresh sample from the workshop, TouchGFX generates codes that cannot be compiled. What should I change?

FMarr.1
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
Alexandre RENOUX
Principal

Hi FMarr.1,

The compiling error you faced seems to be linked to the fatc that you upgraded to the newest version. I believe some functions are no longer supported in the newest version. So following the indication of the workshop but doing your project yourself is the correct way to go I think.

If you touchscreen does not work, it could be that you haven't initialized the touchscreen correctly (I2C not enabled, etc.). Since you are working with H7B3-DISCO, I recommend you to use the Application Template available in the Designer or at least to refer to it.

/Alexandre

View solution in original post

5 REPLIES 5
MM..1
Chief III

"VERY WELL" explain. Try copy here error message!

FMarr.1
Associate II

15:22:42 **** Incremental Build of configuration Debug for project STM32H7B3I_DISCO ****

make -j8 all 

arm-none-eabi-g++ -o "STM32H7B3I_DISCO.elf" @"objects.list" -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m7 -T"C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\STM32H7B3LIHXQ_FLASH.ld" --specs=nosys.specs -Wl,-Map="STM32H7B3I_DISCO.map" -Wl,--gc-sections -static -L"C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc" -L"C:/_SandBox/2020_WShp_GFX/Lab/STM32H7BWorkshop2020_NSA/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -L"C:/STM32H7BWorkshop2020/DryRun/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -L"C:/_Temp/STM32H7BWorkshop2020/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -L"C:/STM32H7BWorkshop2020/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -LC:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group

C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(LCD.o): In function `touchgfx::LCD::drawString(touchgfx::Rect, touchgfx::Rect const&, touchgfx::LCD::StringVisuals const&, unsigned short const*, ...)':

(.text._ZN8touchgfx3LCD10drawStringENS_4RectERKS1_RKNS0_13StringVisualsEPKtz+0x0): multiple definition of `touchgfx::LCD::drawString(touchgfx::Rect, touchgfx::Rect const&, touchgfx::LCD::StringVisuals const&, unsigned short const*, ...)'

Application/User/generated/Texts.o:C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:51: first defined here

C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(Font.o): In function `touchgfx::Font::getStringWidth(unsigned short const*, ...) const':

(.text._ZNK8touchgfx4Font14getStringWidthEPKtz+0x0): multiple definition of `touchgfx::Font::getStringWidth(unsigned short const*, ...) const'

Application/User/generated/Texts.o:C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:14: first defined here

C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(Font.o): In function `touchgfx::Font::getStringWidth(unsigned char, unsigned short const*, ...) const':

(.text._ZNK8touchgfx4Font14getStringWidthEhPKtz+0x0): multiple definition of `touchgfx::Font::getStringWidth(unsigned char, unsigned short const*, ...) const'

Application/User/generated/Texts.o:C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:23: first defined here

C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(Font.o):(.rodata._ZTVN8touchgfx4FontE+0x0): multiple definition of `vtable for touchgfx::Font'

Application/User/generated/Texts.o:(.rodata._ZTVN8touchgfx4FontE+0x0): first defined here

C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(TextProvider.o): In function `touchgfx::TextProvider::initializeInternal()':

(.text._ZN8touchgfx12TextProvider18initializeInternalEv+0x0): multiple definition of `touchgfx::TextProvider::initializeInternal()'

Application/User/generated/Texts.o:C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:46: first defined here

C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(TextProvider.o): In function `touchgfx::TextProvider::getNextLigature(unsigned char)':

(.text._ZN8touchgfx12TextProvider15getNextLigatureEh+0x0): multiple definition of `touchgfx::TextProvider::getNextLigature(unsigned char)'

Application/User/generated/Texts.o:C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:32: first defined here

Application/User/TouchGFX/target/generated/TouchGFXConfiguration.o:(.rodata._ZTV19FrontendApplication[_ZTV19FrontendApplication]+0x30): undefined reference to `touchgfx::Application::requestRedraw()'

Application/User/TouchGFX/target/generated/TouchGFXConfiguration.o:(.rodata._ZTV23FrontendApplicationBase[_ZTV23FrontendApplicationBase]+0x30): undefined reference to `touchgfx::Application::requestRedraw()'

Application/User/TouchGFX/target/generated/TouchGFXConfiguration.o:(.rodata._ZTVN8touchgfx14MVPApplicationE[_ZTVN8touchgfx14MVPApplicationE]+0x30): undefined reference to `touchgfx::Application::requestRedraw()'

collect2.exe: error: ld returned 1 exit status

make: *** [makefile:85: STM32H7B3I_DISCO.elf] Error 1

"make -j8 all" terminated with exit code 2. Build might be incomplete.

15:22:46 Build Failed. 16 errors, 0 warnings. (took 3s.785ms)

FMarr.1
Associate II

the error seems to be in Texts.cpp

By the way, i started from scratch another project, following the indication in the workshop.

It works except the touchscreen does not work. I compare with the workshop code and

missed code in TouchGFXGPIO, this is code generated from TouchGFX. So maybe there miss some

setup i should do to tell TouchGFX i am using touch screen.

Alexandre RENOUX
Principal

Hi FMarr.1,

The compiling error you faced seems to be linked to the fatc that you upgraded to the newest version. I believe some functions are no longer supported in the newest version. So following the indication of the workshop but doing your project yourself is the correct way to go I think.

If you touchscreen does not work, it could be that you haven't initialized the touchscreen correctly (I2C not enabled, etc.). Since you are working with H7B3-DISCO, I recommend you to use the Application Template available in the Designer or at least to refer to it.

/Alexandre

FMarr.1
Associate II

Thanks for reply, i will compare the two versions and try to see where I am wrong.

Regards