2020-12-12 5:38 AM
2020-12-13 6:02 PM
Hi FMarr.1,
The compiling error you faced seems to be linked to the fatc that you upgraded to the newest version. I believe some functions are no longer supported in the newest version. So following the indication of the workshop but doing your project yourself is the correct way to go I think.
If you touchscreen does not work, it could be that you haven't initialized the touchscreen correctly (I2C not enabled, etc.). Since you are working with H7B3-DISCO, I recommend you to use the Application Template available in the Designer or at least to refer to it.
/Alexandre
2020-12-12 5:43 AM
"VERY WELL" explain. Try copy here error message!
2020-12-12 6:24 AM
15:22:42 **** Incremental Build of configuration Debug for project STM32H7B3I_DISCO ****
make -j8 all
arm-none-eabi-g++ -o "STM32H7B3I_DISCO.elf" @"objects.list" -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m7 -T"C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\STM32H7B3LIHXQ_FLASH.ld" --specs=nosys.specs -Wl,-Map="STM32H7B3I_DISCO.map" -Wl,--gc-sections -static -L"C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc" -L"C:/_SandBox/2020_WShp_GFX/Lab/STM32H7BWorkshop2020_NSA/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -L"C:/STM32H7BWorkshop2020/DryRun/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -L"C:/_Temp/STM32H7BWorkshop2020/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -L"C:/STM32H7BWorkshop2020/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -LC:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group
C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(LCD.o): In function `touchgfx::LCD::drawString(touchgfx::Rect, touchgfx::Rect const&, touchgfx::LCD::StringVisuals const&, unsigned short const*, ...)':
(.text._ZN8touchgfx3LCD10drawStringENS_4RectERKS1_RKNS0_13StringVisualsEPKtz+0x0): multiple definition of `touchgfx::LCD::drawString(touchgfx::Rect, touchgfx::Rect const&, touchgfx::LCD::StringVisuals const&, unsigned short const*, ...)'
Application/User/generated/Texts.o:C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:51: first defined here
C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(Font.o): In function `touchgfx::Font::getStringWidth(unsigned short const*, ...) const':
(.text._ZNK8touchgfx4Font14getStringWidthEPKtz+0x0): multiple definition of `touchgfx::Font::getStringWidth(unsigned short const*, ...) const'
Application/User/generated/Texts.o:C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:14: first defined here
C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(Font.o): In function `touchgfx::Font::getStringWidth(unsigned char, unsigned short const*, ...) const':
(.text._ZNK8touchgfx4Font14getStringWidthEhPKtz+0x0): multiple definition of `touchgfx::Font::getStringWidth(unsigned char, unsigned short const*, ...) const'
Application/User/generated/Texts.o:C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:23: first defined here
C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(Font.o):(.rodata._ZTVN8touchgfx4FontE+0x0): multiple definition of `vtable for touchgfx::Font'
Application/User/generated/Texts.o:(.rodata._ZTVN8touchgfx4FontE+0x0): first defined here
C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(TextProvider.o): In function `touchgfx::TextProvider::initializeInternal()':
(.text._ZN8touchgfx12TextProvider18initializeInternalEv+0x0): multiple definition of `touchgfx::TextProvider::initializeInternal()'
Application/User/generated/Texts.o:C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:46: first defined here
C:\2020_ST_GFX_WS\STM32H7BWorkshop2020\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(TextProvider.o): In function `touchgfx::TextProvider::getNextLigature(unsigned char)':
(.text._ZN8touchgfx12TextProvider15getNextLigatureEh+0x0): multiple definition of `touchgfx::TextProvider::getNextLigature(unsigned char)'
Application/User/generated/Texts.o:C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:32: first defined here
Application/User/TouchGFX/target/generated/TouchGFXConfiguration.o:(.rodata._ZTV19FrontendApplication[_ZTV19FrontendApplication]+0x30): undefined reference to `touchgfx::Application::requestRedraw()'
Application/User/TouchGFX/target/generated/TouchGFXConfiguration.o:(.rodata._ZTV23FrontendApplicationBase[_ZTV23FrontendApplicationBase]+0x30): undefined reference to `touchgfx::Application::requestRedraw()'
Application/User/TouchGFX/target/generated/TouchGFXConfiguration.o:(.rodata._ZTVN8touchgfx14MVPApplicationE[_ZTVN8touchgfx14MVPApplicationE]+0x30): undefined reference to `touchgfx::Application::requestRedraw()'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:85: STM32H7B3I_DISCO.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
15:22:46 Build Failed. 16 errors, 0 warnings. (took 3s.785ms)
2020-12-12 6:28 AM
the error seems to be in Texts.cpp
By the way, i started from scratch another project, following the indication in the workshop.
It works except the touchscreen does not work. I compare with the workshop code and
missed code in TouchGFXGPIO, this is code generated from TouchGFX. So maybe there miss some
setup i should do to tell TouchGFX i am using touch screen.
2020-12-13 6:02 PM
Hi FMarr.1,
The compiling error you faced seems to be linked to the fatc that you upgraded to the newest version. I believe some functions are no longer supported in the newest version. So following the indication of the workshop but doing your project yourself is the correct way to go I think.
If you touchscreen does not work, it could be that you haven't initialized the touchscreen correctly (I2C not enabled, etc.). Since you are working with H7B3-DISCO, I recommend you to use the Application Template available in the Designer or at least to refer to it.
/Alexandre
2020-12-13 11:22 PM
Thanks for reply, i will compare the two versions and try to see where I am wrong.
Regards