2020-09-05 12:38 AM
Hi,
I want to know if it's possible to make a 320x480 16Bit LCD as dual buffer, since the internal SRAM of MCU are not continuous!
Is there a trick!
Best Regards
2020-09-05 01:00 AM
One buffer need 307200 continuous ram , second buffer need 307200 too continuous in any place.
2020-09-05 06:16 AM
There is a 512KB continuous ram along some 128K regions, total is 1MB,
So I can only declare one Buffer with this scenario, although my MCU has more RAM!
Is there any trick using MDMA to create a linked list and use dual buffer!
If not, why TouchGFX does not do it for next release!