2019-11-10 6:06 PM
Hello, Now I'm using stm32h747I DISCO to display something.
but when I push Run target button, following Error has occured.
I'll waiting your help.
--------------------------------------------------------------------------------------------------------------------------
Done
Flash
make -f ../gcc/Makefile -j8 flash
STM32CubeProgrammer is placed in Program Files
STM32CubeProgrammer is placed in Program Files (x86)
Converting images
STM32CubeProgrammer is placed in Program Files (x86)
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
extflash.bin - External flash, binary
STM32CubeProgrammer is placed in Program Files (x86)
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
ST-LINK SN : 005000293137510D39383538
ST-LINK FW : V3J3M2
Voltage : 3.26V
SWD freq : 24000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x450
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
Memory Programming ...
Opening and parsing file: target.hex
File : target.hex
Size : 743416 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Error: failed to erase memory
Error: failed to erase memory
Hard reset is performed
gcc/Makefile:334: recipe for target '_extflash_' failed
make[1]: *** [_extflash_] Error 1
make: *** [flash] Error 2
../gcc/Makefile:50: recipe for target 'flash' failed
Failed
Failed
---------------------------------------------------------------------------------------------------------------
2019-11-10 11:47 PM
Hi,
I don't know - It seems like something general (can't erase internal flash). Can you try running STM32CubeProgrammer stand alone and programming it manually? You should have a .hex file in your build/ folder.
Are you getting the same results then?
/Martin
2020-09-09 7:36 PM
I have the same problem when I used STM32H747I DISCO. I have already installed the STM32Cubeprogrammer, but still could not use 'run target' button in TouchGFX. I can download the hex file to the board by STM32 Uitility, but it wastes time.