cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 Weird screen flickering

ktrofimo
Senior III

Using TouchGFX with FreeRTOS I got ​very strange screen flickering issue. For me it looks like broken LTDC buffer addresses, but I have no idea how it could happen.

https://youtu.be/sbEkdzT7yIc

Screen is updated few times every​ second.

And the thing what I can't understand is that code breaking screen has absolutely ​nothing related to LTDC or TouchGFX. For example, I can repair video by disabling one of the FreeRTOS tasks. Or comment out a function that does only some memory buffers initialization and moreover this function is not called for first 10 minutes of firmware uptime. But as soon as I uncomment this function call my screen become crazy. So it is more like kind of static memory issue.

Tasks stacks are placed in separate MCU memory region and all tasks have free stack space.​

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Dear @ktrofimo​ ,

It smells the CM7 speculative access behavior.

Could you please disable the access to memory regions that are not used by your application using the MPU?

For more details about the issue and how to fix it, please refer to the AN4861 "Creating a graphical application with LTDC" / section 4.6 Special recommendations for Cortex-M7 (STM32F7/H7).

Also please refer to this thread: https://community.st.com/s/question/0D53W00001GlRzuSAF/information-about-mpu-settings-for-the-stm32h743

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

2 REPLIES 2
SofLit
ST Employee

Dear @ktrofimo​ ,

It smells the CM7 speculative access behavior.

Could you please disable the access to memory regions that are not used by your application using the MPU?

For more details about the issue and how to fix it, please refer to the AN4861 "Creating a graphical application with LTDC" / section 4.6 Special recommendations for Cortex-M7 (STM32F7/H7).

Also please refer to this thread: https://community.st.com/s/question/0D53W00001GlRzuSAF/information-about-mpu-settings-for-the-stm32h743

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
ktrofimo
Senior III

Yes!

You are correct. My SDRAM memory was not cached and thus it was too slow for my task. Correct cache strategy made big difference!

Thanks!