2021-04-29 9:04 AM
Hello,
I am new to the discovery line up.
I am looking for a ST32H board with fast direct MCU connection LCD similar to the STM32H745-DISCO with 2 MCU DAC outputs. I can't use the codec DAC because the latency is too long. I see only one DAC connected to a pin on the STM32H745-DISCO. Suggestions for a board?
Is there a real fast way for me to check for DAC pins on the MCU and see if they are routed? I am currently just checking pinouts sample projects with cubeMX of various boards and comparing with schematics.
Thanks,
Frank