2019-12-23 12:38 AM
Hi
I am using TouchGFX 4.12.3 with STM32F746G-DISCO Board.
I have already installed STLink and STCubeProgrammer.
I am able to GUI run on simulator but not on target .
Please check below logs.
--
Thanks
Gurpreet Singh
2019-12-23 12:40 AM
Run Target
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j10
Converting images
Done
Post Generate
touchgfx update_project --project-file=../EWARM/MyApplication_3.ewp --gui-group-name=Application/User/TouchGFX/gui --generated-group-name=Application/User/TouchGFX/generated && touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Compile
make -f ../gcc/Makefile -j8
Converting images
Compiling TouchGFX/gui/src/screen1_screen/Screen1Presenter.cpp
Compiling TouchGFX/generated/fonts/src/Font_verdana_20_4bpp_0.cpp
Compiling TouchGFX/gui/src/common/FrontendApplication.cpp
Compiling TouchGFX/gui/src/screen1_screen/Screen1View.cpp
Compiling TouchGFX/generated/gui_generated/src/screen1_screen/Screen1ViewBase.cpp
Compiling TouchGFX/generated/fonts/src/Font_verdana_40_4bpp_0.cpp
Compiling TouchGFX/gui/src/model/Model.cpp
Compiling TouchGFX/generated/gui_generated/src/common/FrontendApplicationBase.cpp
Compiling TouchGFX/generated/fonts/src/GeneratedFont.cpp
Compiling TouchGFX/generated/fonts/src/Kerning_verdana_40_4bpp.cpp
Compiling TouchGFX/generated/fonts/src/Table_verdana_10_4bpp.cpp
Compiling TouchGFX/generated/fonts/src/Kerning_verdana_20_4bpp.cpp
Compiling TouchGFX/generated/fonts/src/FontCache.cpp
Compiling TouchGFX/generated/fonts/src/Kerning_verdana_10_4bpp.cpp
Compiling TouchGFX/generated/fonts/src/Font_verdana_10_4bpp_0.cpp
Compiling TouchGFX/generated/fonts/src/CachedFont.cpp
Compiling TouchGFX/generated/fonts/src/Table_verdana_40_4bpp.cpp
Compiling TouchGFX/generated/fonts/src/Table_verdana_20_4bpp.cpp
Compiling TouchGFX/generated/fonts/src/ApplicationFontProvider.cpp
Compiling TouchGFX/generated/images/src/__designer/Blue_Buttons_Round_Edge_small.cpp
Compiling TouchGFX/generated/images/src/__designer/Blue_Buttons_Round_Edge_small_pressed.cpp
Compiling TouchGFX/generated/images/src/BitmapDatabase.cpp
Compiling TouchGFX/generated/texts/src/TypedTextDatabase.cpp
Compiling TouchGFX/generated/texts/src/Texts.cpp
Compiling Middlewares/ST/TouchGFX/touchgfx/os/OSWrappers.cpp
Compiling TouchGFX/target/STM32F7Instrumentation.cpp
Compiling Core/Src/main.cpp
Compiling TouchGFX/target/STM32F7TouchController.cpp
Compiling TouchGFX/target/STM32F7DMA.cpp
Compiling TouchGFX/target/STM32F7HAL.cpp
Compiling TouchGFX/target/GPIO.cpp
Compiling TouchGFX/target/HW_Init.cpp
Compiling TouchGFX/target/BoardConfiguration.cpp
In file included from Core/Src/main.cpp:53:0:
Core/Src/main.cpp: In function 'int main()':
Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.h:470:54: warning: ISO C++ forbids converting a string constant to 'char*' [-Wwrite-strings]
{ #name, (thread), (priority), (instances), (stacksz)}
^
Core/Src/main.cpp:176:5: note: in expansion of macro 'osThreadDef'
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 4096);
^~~~~~~~~~~
Compiling Middlewares/Third_Party/FreeRTOS/Source/croutine.c
Compiling Middlewares/Third_Party/FreeRTOS/Source/list.c
Compiling Middlewares/Third_Party/FreeRTOS/Source/tasks.c
Compiling Middlewares/Third_Party/FreeRTOS/Source/queue.c
Compiling Middlewares/Third_Party/FreeRTOS/Source/timers.c
Compiling Middlewares/Third_Party/FreeRTOS/Source/portable/MemMang/heap_2.c
Compiling Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1/port.c
Compiling Drivers/BSP/STM32746G-Discovery/stm32746g_discovery.c
Compiling Drivers/BSP/Components/ft5336/ft5336.c
Compiling Drivers/BSP/STM32746G-Discovery/stm32746g_discovery_ts.c
Compiling Drivers/BSP/STM32746G-Discovery/stm32746g_discovery_qspi.c
Compiling Drivers/BSP/STM32746G-Discovery/stm32746g_discovery_sdram.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_cortex.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_dma.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_dma2d.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_gpio.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_dma_ex.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_i2c.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_i2c_ex.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_ltdc.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_nor.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_pwr_ex.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_sdram.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc_ex.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_sd.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim_ex.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_qspi.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_pwr.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_crc_ex.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_crc.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rtc.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rtc_ex.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_uart.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_fmc.c
Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_sdmmc.c
Compiling Core/Src/system_stm32f7xx.c
Compiling Core/Src/freertos.c
Compiling Core/Src/stm32f7xx_hal_msp.c
Compiling Core/Src/stm32f7xx_hal_timebase_tim.c
Compiling Core/Src/stm32f7xx_it.c
Compiling ASM Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/gcc/startup_stm32f746xx.s
Compiling Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.c
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
extflash.bin - External flash, binary
Done
Flash
make -f ../gcc/Makefile -j8 flash
Converting images
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
extflash.bin - External flash, binary
/usr/bin/sh: C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ST-LINK_CLI.exe: No such file or directory
gcc/Makefile:318: recipe for target '_extflash_' failed
make[1]: *** [_extflash_] Error 127
../gcc/Makefile:50: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
2019-12-25 4:45 AM
Wouldn't it be a good idea to update the firmware on your ST-link first? press the big blue 'firmware upgrade' button and see if that works.
the examples in TouchGFX designer should work out of the box. do they?
2020-05-27 5:46 AM
Did you find the solution? if yes please post it. thanks