2019-12-04 10:39 PM
I follow same as in this video https://www.youtube.com/watch?v=ZQA2lAsIdZA but not showing UI template in display, its show only black screen, when build the project there is no errors and warnings,
2019-12-05 12:35 AM
the video is made for the parallel interface (LTDC) on the 746 and not the DSI interface of the 769i. I am the one who made it..
I would imagine that you have to look into the setup of the DSI interface and figure out the settings that are somehow wrong in the CubeMX generation. Have a look at how the interface is configured in the TouchGFX generated code
2019-12-05 1:25 AM
i also tried in stm32f429I, it is LTDC interface, after flash the code in this discovery board it shows dots
2019-12-05 1:33 AM
does it work with a project generated using TouchGFX designer? If so, you'll have to look into the display settings in that project and find the differences
2019-12-05 1:39 AM
it worked in touchgfx by run target
2019-12-05 3:53 AM
how can i change the display settings in the project
2019-12-05 4:22 AM
If you followed the video you will have access to the display setup in the .ioc file (opening the cubeMX settings).
These settings should be written in the TouchGFX config/init methods.