cancel
Showing results for 
Search instead for 
Did you mean: 

[SOLVED] STM32F469I-Disco and TouchGfx 4.20.0. I bought STM32F469IDisco. Version MB1189-F469NIH6-B08-A222300689. When I try start new project with TouchGFX, result is black screen.

SPrik
Associate II

I tried both "Run Target" from TouchGFX Designer, and Cube IDE (Cube MX) compile / debug result is black screen. Compile, debug and run is without errors.

36 REPLIES 36

Thank you very much. This fixed my issue.

Hi Romain

I think this is a part of EmbDev's fix. So yes it looks like the soultion for the TouchController initialization issue. Thanks.

Thank you for sharing your example, it is very helpful to all of us :thumbs_up:

/Romain

Can I get a demo project? E-mail address is eyefor@naver.com. Thank you.

Osman SOYKURT
ST Employee

Hello,

A new TBS is now available on TouchGFX Designer 4.21.0 for this STM32F469I-Disco $AU1 revision (B08)

0693W00000Y7iYHQAZ.png 

It should resolve the issue with the black screen.

/Osman

Osman SOYKURT
ST Software Developer | TouchGFX
SPrik
Associate II

Thanks Oskt for reply.

It is working....I think,,problem with this LCD and this board is solved.

It is working, Thanks