2022-10-22 9:57 AM
I tried both "Run Target" from TouchGFX Designer, and Cube IDE (Cube MX) compile / debug result is black screen. Compile, debug and run is without errors.
Solved! Go to Solution.
2022-11-30 5:46 AM
Thank you very much. This fixed my issue.
2022-11-30 5:53 AM
Hi Romain
I think this is a part of EmbDev's fix. So yes it looks like the soultion for the TouchController initialization issue. Thanks.
2022-11-30 8:21 PM
Thank you for sharing your example, it is very helpful to all of us :thumbs_up:
/Romain
2022-12-29 4:23 PM
Can I get a demo project? E-mail address is eyefor@naver.com. Thank you.
2023-01-09 2:42 AM
Hello,
A new TBS is now available on TouchGFX Designer 4.21.0 for this STM32F469I-Disco $AU1 revision (B08)
It should resolve the issue with the black screen.
/Osman
2023-01-09 9:22 AM
Thanks Oskt for reply.
It is working....I think,,problem with this LCD and this board is solved.
2023-01-09 1:25 PM
It is working, Thanks