cancel
Showing results for 
Search instead for 
Did you mean: 

SDRAM 위치�? 배열�?� 잡아 DCMI�?� �?��?�터를 넣으려고 하는�?� SDRAM 설정 후 DCMI 설정�?� 하면 배열내 �?��?�터가 변화합니다.

SKoh.12
Associate II
 
2 REPLIES 2
AScha.3
Chief III

यदि भवान�? आङ�?ग�?लभाषायां लिखति तर�?हि शीघ�?रं साहाय�?यं प�?राप�?न�?यात�?।

If you feel a post has answered your question, please click "Accept as Solution".

>>I am trying to put DCMI data by holding an array in the SDRAM location, but if I set DCMI after SDRAM setting, the data in the array changes.

What part, on what board, with what software?

Kind of suggests that there are pins in common between the two, check schematics / manuals, and any README.TXT related to project.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..