2020-09-03 02:23 AM
Hi,
I am using the following screen and CPU : 4DLCD-70800480 and STM32F746BGT.
I configured the LTDC and TouchGFX parameter settings but the screen tears ...
I have attached all the configuration.
Best Regards
Solved! Go to Solution.
2020-09-08 12:37 AM
Your clock tree seems strange to me.
The LCD-TFT clock and the SDMMC clock looks wrong. If you look at the F746G-DISCO AT, the LCD-TFT clock is at 9.6 MHz. Try with this value and also try to avoid having clocks with a high number of decimals in any case.
/Alexandre
2020-09-07 05:07 AM
Hello,
Did you have a look at the F746G-DISCO Application Template in the Designer ?
What kind of tearing do you notice ? Could you provide a picture of the issue ?
/Alexandre
2020-09-07 06:05 AM
2020-09-08 12:37 AM
Your clock tree seems strange to me.
The LCD-TFT clock and the SDMMC clock looks wrong. If you look at the F746G-DISCO AT, the LCD-TFT clock is at 9.6 MHz. Try with this value and also try to avoid having clocks with a high number of decimals in any case.
/Alexandre
2020-09-08 07:08 AM
Hi,
It works with 9.6 MHz but the screen flickers.
The best for this screen is 17 MHz.
Thanks !