2023-03-30 10:19 AM
Hello,
I just encountered "failed to download Segment[1]" error in the middle of tough gfx project downloading.
Demo Board : STM32U5A9J-DK
CubeProgrmmer version : 2.13.0
TouchGFX version : 4.21.3
Error message capture
I found that toughgfx is using the Cubeprogrammer tool for binary downloading.
So I searched if the CubeProgrammer has the STM32U5A9J-DK ext-flash binary but can't find for it.
Seems tool update is needed.
I also found that cuscumized ext-flashing binary can be created with IAR compiler.
https://github.com/STMicroelectronics/stm32-external-loader
But I don't have the IAR :(
So it would be appreciated if to provide the patch file or update the CubeProgrammer ASAP.
2023-03-31 2:00 AM
Same identical problem me too, using same board and same configuration.
With a little amount of space of images in external memory, like one or two little images in project, it work.But with a large image and large amount of external memory used not work.
Any suggestion ?
Heeeeelp please :o
2023-04-11 12:22 AM - edited 2023-11-20 9:05 AM
I have solved !
The problem is with STM32CubeProgrammer v2.13.0, the internal one used by TouchGFXDesigner and STMCubeIDE.
I have found the folder where STM32CubeProgrammer v2.13.00 is installed and I have copied over the old folder where STM32CubeProgrammer v2.10.00 was used.
Now TouchGFXDesigner and STMCubeIDE working fine with STM32U5A9j.
2023-04-11 2:37 AM
We identified the issue and we're working on it. Our apologies for this inconvenience. As a workaround, for now, you can use STM32CubeProgrammer v2.12.0 to flash your STM32U5A9J-DK board.
We'll make sure to patch this in the 2.14.0 version of STM32CubeProgrammer.
/Osman
2023-04-11 3:20 AM
Thanks for your support. I will try the temp solution as you guided. BTW, when the 2.14 will be released?
2023-04-11 3:21 AM
Hey~ Good job.
Thanks for your effort.
I will try it.
2023-04-11 5:01 AM
No I don't, no official date was communicated yet, but I'll keep you updated when I'll have more info about this subject.
/Osman
2023-04-11 6:04 AM
I see.
Thank you~:thumbs_up: