cancel
Showing results for 
Search instead for 
Did you mean: 

Question about the TouchGFX interface

rhine1012
Visitor

Hi, CARHER 

I just want to know what is the software you show in the picture?

Where to download it?

thank you.

post created based on a command posted on an old thread. here is the picture mentioned by the customer: 

STTwo32_0-1738682566316.png

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @rhine1012 and welcome to the ST community.

I've created this post based on your comment on an old thread with all necessary edits. For your question, this is TouchGFX interface. You can download it using this link: TouchGFXDesigner - TouchGFX is delivered as an X-Cube-TouchGFX package - STMicroelectronics

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @rhine1012 and welcome to the ST community.

I've created this post based on your comment on an old thread with all necessary edits. For your question, this is TouchGFX interface. You can download it using this link: TouchGFXDesigner - TouchGFX is delivered as an X-Cube-TouchGFX package - STMicroelectronics

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.