cancel
Showing results for 
Search instead for 
Did you mean: 

Pre flashed firmware in STM32U575ZI-NUCLEO-AZ2

mdalal
Associate III

Hi,

I want to get the access to the default pre flashed firmware image flashed while receiving STM32U575ZI-NUCLEO-AZ2 eval board. Can you share that whole firmware project along with the source code? 

Also, whether the UI is built using TouchGFX? If yes, is it also possible to share the TouchGFX project as well for the default firmware on the eval board?

Thanks,

Mehul

5 REPLIES 5
STTwo-32
ST Employee

Hello @mdalal 

First, are you using the NUCLEO-U575ZI-Q or the STM32U575I-EV.If, you are using the nucleo board, i don't know any graphic demo for this board since it does not came with a screen. If you are tooking about the evaluation product, you can take a look at the demonstration from this link

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

My bad, I am using STM32U575I-EV. Are there any touchgfx project for the baord available? Or I should be using below link for reference?

https://github.com/STMicroelectronics/STM32CubeU5/tree/main/Projects/STM32U575I-EV

I did not see any touchgfx reference for UI images in there.

Hello @mdalal ,

I don't think the default demo source code is provided in public. It's only provided as binary in this link.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Christian N
ST Employee

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

SofLit
ST Employee

Same question here.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.