Skip to main content
DavidEGrayson
Associate II
April 1, 2025
Solved

Derivation of 12-character USB serial number in STM32C0's system bootloader

  • April 1, 2025
  • 1 reply
  • 521 views

How does the bootloader in the STM32C071 system memory generate its 12-character USB serial number string descriptor (e.g. "205537C24236")?  I notice some similarities between this serial number and the 96-bit unique device ID at address 0x1FFF7550, but overall they look very different.  I'm asking because I would like my firmware to use the same serial number as the bootloader, and being able to use a compact serial number would be beneficial as well.

Here are some examples of the 96-bit unique ID (hex formatted, with dashes after every 2 bytes) and the corresponding 12-character USB serial number:

1: 7A00-2500-0150-3642-4837-3020, 205537C24236
2: 7B00-5700-0150-3642-4837-3020, 208737C34236
3: 7B00-2700-0150-3642-4837-3020, 205737C34236
4: 7B00-8100-0150-3642-4837-3020, 20B137C34236

I looked at the documentation of the unique ID in RM0490, section 30.1, but that documentation was partially incorrect and did not help.

 

This topic has been closed for replies.
Best answer by DavidEGrayson

I figured it out!  I found a useful thread on this forum and it appears the STM32C0's bootloader is behaving the same was as the STM32F4, so you can generate the 16-bit words needed by doing:

uint16_t * const uid = (uint16_t *)UID_BASE;

uint16_t words[] = { uid[1] + uid[5], uid[0] + uid[4], uid[3] };

I would have just deleted my original post if I could find the option for that.

1 reply

DavidEGrayson
DavidEGraysonAuthorBest answer
Associate II
April 1, 2025

I figured it out!  I found a useful thread on this forum and it appears the STM32C0's bootloader is behaving the same was as the STM32F4, so you can generate the 16-bit words needed by doing:

uint16_t * const uid = (uint16_t *)UID_BASE;

uint16_t words[] = { uid[1] + uid[5], uid[0] + uid[4], uid[3] };

I would have just deleted my original post if I could find the option for that.