2024-10-21 11:28 PM
I am trying to use the ChromART accelerator foor my touchgfx project hacing the display on the SPI line.
However, while I am enabling the TouchGFX, I also wanted to enable the use of ChromART DMA for a grescale display. But the, the STMCubeMX does not allow me to enable the ChromART if I select "BW" or "Gray 2" or "Gray 4" pxel format. Kinldy suggest.
2024-10-22 9:08 AM
Hello @mdalal
To use the DMA2D Accelerator (ChromART), you have to select one of the supported Pixel Format (and Enable DMA2D for sure). For BW, Gray2 and Gray4, it seems to be the not supported Pixel Formats.
Best REgards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-22 8:55 PM
Hi,
When you say "it seems", is it conformed that the tool indeed does not support the ChromART for Greayscale or you are not sure about it?
Also, where in the manual is it written that BW, Grey2 and Gray4 cannot be supported by ChromeART and why?
2024-11-01 10:04 AM
Hello @mdalal
Sorry for my late reply. Here are the Supported formats (with TouchGFX) for the DMA2D:
You can find this table and more on this link: TouchGFX on NeoChrom/NeoChromVG | TouchGFX Documentation
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.