Skip to main content
Senior
December 4, 2024
Solved

FATFS Failure with FreeRTOS

I am using the STM32H7B3I-DK for my project. I am trying to integrate uSD card usage with a touchgfx program. I have gotten a simple write to a file working on a non rtos project; however, when I use it in my project with RTOS I keep getting a hard fault. I had to make the SDMMC have a clock divider of 2 to get it to work on non-rtos. Are there some conflicts with FreeRTOS that I need to be considering?

Here is the code I am using in both:

 

FRESULT res; /* FatFs function common result code */
UINT byteswritten, bytesread; /* File write/read counts */
uint8_t wtext[] = "STM32 FATFS works great!"; /* File write buffer */
uint8_t rtext[_MAX_SS];/* File read buffer */

[...]

BYTE work[4096]; // Work area for formatting
 /* USER CODE BEGIN 5 */
	 printf("Starting\r\n");
	 if(f_mount(&SDFatFS, (TCHAR const*)SDPath, 1) != FR_OK)
	 {
		 printf("Failed to mount -- Formatting\r\n");
		 if (f_mkfs(SDPath, FM_FAT32, 0, work, sizeof(work)) != FR_OK) {
			 printf("Failed to format SD card.\r\n");
			 return;
		 } else {
			 printf("SD card formatted to FAT32 successfully.\r\n");
		 }
	 }


	 //Open file for writing (Create)
	 if(f_open(&SDFile, "STM32.TXT", FA_CREATE_ALWAYS | FA_WRITE) != FR_OK)
	 {
	 printf("Failed on open\r\n");
	 }
	 else
	 {
	 //Write to the text file
	 res = f_write(&SDFile, wtext, strlen((char *)wtext), (void *)&byteswritten);
	 if((byteswritten == 0) || (res != FR_OK))
	 {
	 printf("Failed on write\r\n");
	 }
	 else
	 {
	 f_close(&SDFile);
	 }
	 }


	 f_mount(&SDFatFS, (TCHAR const*)NULL, 0);
	 printf("Done\r\n");

 

  

This topic has been closed for replies.
EthanMankinsBest answer
Senior
December 4, 2024

I have solved the hard fault by changing task priority; however, I fail f_open() and f_mount() with a NO_FILE_SYSTEM, even after f_mkfs() succeeds.

2 replies

EthanMankinsAuthorBest answer
Senior
December 4, 2024

I have solved the hard fault by changing task priority; however, I fail f_open() and f_mount() with a NO_FILE_SYSTEM, even after f_mkfs() succeeds.

Andrew Neil
Super User
December 4, 2024

@EthanMankins wrote:

I have solved the hard fault by changing task priority; 


Great - so please mark that as the solution:

https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

 


@EthanMankins wrote:

however, I fail f_open() and f_mount() with a NO_FILE_SYSTEM, even after f_mkfs() succeeds.


New thread for that:

https://community.st.com/t5/stm32-mcus-embedded-software/fatfs-rtos/td-p/750564

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.