cancel
Showing results for 
Search instead for 
Did you mean: 

Noob question. I have STM32H7B3I-DK and need to connect and grab info from the internet. Need a sample project.

TCygan
Associate II

So I'm new to this development.  I have STM32H7B3I-DK and need to connect to wifi/Internet and grab some data. I've experimented with TouchGFX Designer and there are templates that I like, especially the lens widget. Here are my questions:

  1. Is there a sample project that I can use?
  2. Would this entail the use of TouchGFX and some other software? Perhaps CubeIDE?
  3. Is there a good pdf or video on how to use TouchGFX with CubeIDE?

Thank you!!

**FYI; I'm running TouchGRX 4.15.0, CubeIDE 1.5.0, CubeProgrammer 2.5

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello @TCygan​ ,

You can follow the TouchGFX getting started and create your project from TouchGFX Designer with the right application template, then launch STM32CubeIDE and open the project generated (in the directory C:\TouchGFXProjects)

You have also the TouchGFX tutorials and TouchGFX MOOC to start your project,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen