cancel
Showing results for 
Search instead for 
Did you mean: 

Linker error with provided ARMCLANG library from TouchGfx 4.14.0

jimmii
Senior II

Hi @Martin KJELDSEN​ 

I just updated to 4.14.0. Now I get the linker as I got them in this thread (the problem was the short enums/wchar settings) https://community.st.com/s/question/0D50X0000AlgbG2SQI/arm6-compiler-support

I can see that the armclang lib that comes with 4.14.0 is smaller than the version you provided in the thread.

Any thoughts?

Cheers /jimmii

43 REPLIES 43

Hey @Martin KJELDSEN​ 

Looks good. (At least for my project).

Thanks a lot.

/jimmii

Hi @Martin KJELDSEN​ 

Would you be so kind to provide me with the new library for 4.16.0 as you did for the last versions?

Thanks a lot.

Hi Jimmii,

Yes i would be so kind - I'll put it on my list.

/Martin

Hi @Martin KJELDSEN​ , how does it look? Did you have any chance to compile the library for me?

Thanks.

​I'll do it now - Just brushing up on your compiler settings

 

Let me know how it works for you @Roman Schläpfer​ 

-xc -std=c99 --target=arm-arm-none-eabi -mcpu=cortex-m7 -mfpu=fpv5-sp-d16 -mfloat-abi=hard -c -fno-rtti -funsigned-char -fshort-enums -fshort-wchar -mlittle-endian -gdwarf-3 -Oz -ffunction-sections

/Martin

Thanks @Martin KJELDSEN​ , I ill have a look as soon as I'm back from vacation.

​Ok @Roman Schläpfer​ - Are you saying working on TouchGFX projects is not like vacation? Have a great time off :D