cancel
Showing results for 
Search instead for 
Did you mean: 

LCD touch is strange

DKim.35
Associate II

Hello experts. Let me ask you a question.

I compiled the code made through TouchGFX with IDE and downloaded it to the board with Programmer.

If you touch after disconnecting to check, the touch does not work.

However, if I connect and then disconnect again, the touch works fine. What is the problem?

Additionally, even when debugging in the IDE compiler, touch works fine.

2 REPLIES 2
MM..1
Chief III

Strange is your description . Try first use search here enter "touch" and ...

for example TouchGFX generated project is not worked on STM32F746G-DISCO(C01) (Only the "touch screen" doesn't work.)

Osman SOYKURT
ST Employee

Hello DKim.35,

Indeed, the description of your issue reminds me an other thread on the forum.

Which board do you use ? And which version of TouchGFX Designer do you use ?

/Osman

Osman SOYKURT
ST Software Developer | TouchGFX