2022-12-04 01:07 AM
Hello experts. Let me ask you a question.
I compiled the code made through TouchGFX with IDE and downloaded it to the board with Programmer.
If you touch after disconnecting to check, the touch does not work.
However, if I connect and then disconnect again, the touch works fine. What is the problem?
Additionally, even when debugging in the IDE compiler, touch works fine.
2022-12-04 07:05 AM
Strange is your description . Try first use search here enter "touch" and ...
for example TouchGFX generated project is not worked on STM32F746G-DISCO(C01) (Only the "touch screen" doesn't work.)
2022-12-08 12:58 AM