2019-05-06 07:56 AM
I have created a few test project for TouchGFX V4.10. The projects build without any error and could be loaded to a ATM32F7 disco boards. What i am mussing are the Keil uVision project files as well as the directory for a created project. The IAR project files as well as the directory have been created for each project. Is there a setting to enable the creating of the Keil files?
Keil uVision V5.27.1.0 is installed on the PC to be used.
2019-05-07 12:12 AM
Hi @CRoes.4,
How are you creating these projects? Through the application templates in the designer? For certain versions of ATs (application templates) there are no Keil projects. If you use the latest CubeMX you should be able to create your missing Keil projects with TouchGFX.
Let me know,
Best regards,
Martin
2019-05-14 06:35 AM
Any update on this, @CRoes.4 ?
/Martin