cancel
Showing results for 
Search instead for 
Did you mean: 

Integration of TouchGFX with an External Display via. the B-LCDAD-HDMI1 board for the STM32F769-Discovery

Michael Chinnery
Associate

Hi all,

I am currently using the STM32F769-Discovery board.

I am looking to display a GUI designed with TouchGFX Designer (4.20.0) on an external screen via. the B-LCDAD-HDMI1 board.

The display I am using is the 7inch Capacitive Touch Screen LCD (7inch Capacitive Touch Screen LCD (C), 1024×600, HDMI, IPS, Low Power Consumption (waveshare.com))

Up till now I have been able to implement the LCD_DSI_VideoMode_SingleBuffer example project such that the screen shows the alternating images as intended. However, I have struggled with the LCD_DSI_CmdMode_DoubleBuffer due to makefile errors.

When i've attempted to implement the elements of the example which relate to displaying on the external screen i've had difficulties identifying what to send to the video buffer from TouchGFX elements.

Has anyone had any experiences similar to this and able to lend a hand?

0 REPLIES 0