2019-03-14 11:14 AM
2019-03-14 02:49 PM
Hi @David.Yves,
Just change it under "Application Directory" when creating an application. Subsequent applications will be placed here.
/Martin
2019-03-16 10:56 AM
2020-05-21 02:14 PM
Version 4.13.0 still has this issue (default directory, not tried spaces in directory names). Given a full C drive, TouchGFX has selected installation on the D drive, yet the Application Directory defaults to C:\TouchGFXProjects. This is an unfortunate usability flaw in an attractive UI
I have also tried loading an image file with a space in the file name - the UI reports an error and allows you to load a different image file (e.g. copy and change the name of the one previously selected, t.b.h. I couldn't see a way to undo adding the image), but leaves the file with a space in loaded into the project (which stops the simulator or target running, but Generate Code still works and reports no errors - only a red outline on the Images button). This is another usability glitch - I think the application could benefit from being tested by someone unfamiliar with it.
As a developer I know how easy it is to always test in the same manner - having someone else test your application / module tends to reveal actions that the developer would never consider the user doing. Having an 'idiot user' test an application (particularly one with an attractive UI, as there's less 'common knowledge' of how it works) is very useful
2020-05-26 02:46 AM
Hi Piers,
I agree with you. It's something we've not prioritized for a while because there were more pressing matters, but i've raised the issues again internally. Thanks for your feedback!
/Martin
2020-11-03 11:26 AM
This remains an annoying problem for me in version 4.15.0.
2020-11-04 12:46 AM
Hi, I think it's time to raise this again internally. Consider it done :)
2020-11-09 03:36 PM
That's great news @Martin KJELDSEN . Thank you.
2020-11-09 11:54 PM
No problem. Given an increased focus on ransomware and that kind of thing, it's important to be able to store your work in a place that is backed up without having to turn every project into a git repository.
2020-11-10 06:32 PM
@Martin KJELDSEN Funny, that brings up another issue. My projects directory is a git repo but it's also within DropBox locally.
Dropbox forces a space in the directory name. So I have to drive map the git repo subdirectory.
This is a TouchGFX exclusive issue among my commonly used programs.