cancel
Showing results for 
Search instead for 
Did you mean: 

I cannot create any project or run simulator or generate cod

Fadi.Albaghdadi
Associate III

Generate Code

  Generate

    Done

  Generate Assets

    make -f simulator/gcc/Makefile assets -j10

    The system cannot find the path specified.

    'B' is not recognized as an internal or external command,

    operable program or batch file.

    The system cannot find the path specified.

    The system cannot find the path specified.

    The system cannot find the path specified.

    Failed

  Failed

5 REPLIES 5
Romain DIELEMAN
ST Employee

Hi,

Could you share the path of your project ? Are there any space or "uncommon" characters somewhere ?

Could you also specify the version of TouchGFX you are using ? Are you creating a project with an application template for a specific board or a UI template ?

/Romain

Thank you very much. You can log in to my computer and see the problem anydesk

I am using a blank project in addition I also tried with a template

I find the same problem

email: fadi.albaghdade@gmail.com

I know there has been people facing similar issues with Turkish language settings on their computer, I cannot remember the exact reason but it was due to some characters not recognized in the folder path of the projects. Please try creating a project directly in the /C folder or in /C/TouchGFXProject. I'll try to find the previous posts of people facing the same issue

/Romain

My computer is in English and I use the default path for the program

The problem is that it was working fine, but I don't know what happened to it

But I also tried the program on another computer and found the same problem

He's telling you to use some thing other than the default, which might be a user directory or other with odd characters in it.

Use a simple path for the program and the repository, etc. ie C:\TouchGFX

The above error is also complaining about a "B" option/command, see if you can see any build output or dialogs referring to what specific path is problematic. Perhaps go look at the makefile it is invoking, and show the directory that is in.

It is very hard to debug things with the level of detail/specificity provided.

Have your IT guy review the situation and the installation method.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..