2020-06-04 9:36 AM
Hello!
Sorry I am new to stm32 and TouchGfx.
I am currently reading from SPI and want to relay that data to the screen using:
Unicode::snprintf(textCounterBuffer, 10, "%d", finalData);
textCounter.invalidate();
my problem is that the finalData is a decimal figure and the decimal gets cut off.
When I try to display the raw data number from my spi it displays fine and is a uint8_t variable. I need to adjust this number using:
finalData = (spiRxBuf/4096)*100;
but as I said before the screen does not display the number properly.
2020-06-04 11:28 AM
%d is integer, for a floating point double use %lf
2020-06-04 12:08 PM
Wow, thanks, I feel stupid for missing that.
Thank you!
2020-06-04 12:30 PM
sorry, I changed it to %lf and when I click the button on the screen the program locks up.
Any thoughts? Maybe its the way I have my wildcard?
2020-06-04 2:32 PM
Make sure the buffer is deep enough to hold the string and terminate it.
Sorry not using TouchGFX / CubeIDE
2020-06-08 12:59 AM
Hi, it is because you are using snprintf() and not snprintfFloat() (or floats).
%f is not supported by the "normal" snprintf() because floats are converted to doubles when given as parameters in a variable argument list (va_list).
/Romain
2020-06-08 8:23 AM
I apologize I should have closed this thread, I found a page from TouchGfx website that helped with the snprintfFloat().
I am now having a strange crash though, the data that I receive through SPI needs to run through a formula before it is useful, but when I use the SPI data that is saved as int result:
int result = ((highByte & 0x1f) << 7) | ((lowByte >> 1));
and send the finalData from that to:
Unicode::snprintfFloat(textCounterBuffer, 50, "%.4f", finalData);
I get a crash.
BUT when I send a regular int, lets say, int x = 2000. To the formula:
float finalData = (float)result*3.3;
finalData /= 4096;
then put it into:
Unicode::snprintfFloat(textCounterBuffer, 50, "%.4f", finalData);
it runs just fine and I get the number I expect to the screen.
2020-06-09 12:40 AM
Hi,
First are you sure of what you are receiving? If your process works with a set int then the issue comes from what you are receiving or how you are handling it.
Could you share your formula or code as well, it is a bit confusing.
/Romain
2020-06-09 6:18 AM
Sorry, yes here is my code:
//put CS low
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);
//Transmit Data
spiTxBuf[0] = 0x05;
HAL_SPI_Transmit(&hspi2, spiTxBuf, 1, 10);
//read the data
HAL_SPI_Receive(&hspi2, &spiRxBuf, 1, 10);
highByte = spiRxBuf;
HAL_SPI_Receive(&hspi2, &spiRxBuf, 1, 10);
lowByte = spiRxBuf;
int result = ((highByte & 0x1f) << 7) | ((lowByte >> 1));// & 0x7f);
float finalData = (float)result*3.3;
finalData /= 4096;
//bring CS high
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);
Unicode::snprintfFloat(textCounterBuffer, 50, "%.4f", finalData);
While is was using the snprintf for %d I was able to print the int result perfectly fine, which led me to believe this was an int value.
2020-06-10 1:20 AM
So what do you get when you do:
int result = ((highByte & 0x1f) << 7) | ((lowByte >> 1));// & 0x7f);
Unicode::snprintf(textCounterBuffer, 50, "%d", result);
//float finalData = (float)result*3.3;
//finalData /= 4096;
//bring CS high
//HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);
//Unicode::snprintfFloat(textCounterBuffer, 50, "%.4f", finalData);
if the data is what you expected, uncomment/debug step by step to see if it is a calculation problem or something else.