2024-12-16 10:01 PM
Hi there,
In my touchGFX project, I import an SVG file.
I can compile and simulate the UI page using TouchGFX Designer, which works as expected.
However, after I finished the design in TouchGFX Designer and tried to compiler the project by MDK-ARM, the following error was present:
(When I delete the SVG object in TouchGFX Designer, everything works well again.)
I don't know what this means, how do I resolve it?
Thanks for your help!
Solved! Go to Solution.
2024-12-17 12:58 AM
2024-12-17 12:58 AM
2024-12-17 07:11 AM
Hello @Junde ,
Could you check if it works when compiling and flashing from TouchGFX Designer?
Maybe there is a missing include file or library path in your IAR project?
Regards,
2024-12-17 06:02 PM
@ferro Thank you
this resolved my error!
2024-12-17 06:06 PM
@GaetanGodart thanks for your reply
It can work well with the touchGFX Designer in simulation mode.
My question can be resolved by enabling "Vector Rendering" in cubeMx.