Skip to main content
Sany
Associate III
December 17, 2024
Solved

STM32U575 and TouchGFX ends in FaultHandler

  • December 17, 2024
  • 7 replies
  • 1394 views

Hello Everyone,

 

I have a STM32U575 CPU, with a ILI9341 LCD Display, this works fine with a STM32F4, but i am upgraded my PCB to a STM32U575 and got Problems with the SPI...

my main.c code:

 

int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_GPDMA1_Init();
 MX_CRC_Init();
 MX_SPI1_Init();
 MX_UART4_Init();
 MX_UART5_Init();
 MX_USB_OTG_FS_USB_Init();
 MX_I2C1_Init();
 MX_USART3_UART_Init();
 MX_TIM2_Init();
 MX_ICACHE_Init();
 MX_RTC_Init();
 MX_TouchGFX_Init();
 /* USER CODE BEGIN 2 */
 HAL_GPIO_WritePin(LCD_BACKLIGHT_GPIO_Port, LCD_BACKLIGHT_Pin, GPIO_PIN_SET);

 ILI9341_Init();

 HAL_TIM_Base_Start_IT(&htim2);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 MX_TouchGFX_Process();
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_LSI
 |RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
 RCC_OscInitStruct.LSIState = RCC_LSI_ON;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_0;
 RCC_OscInitStruct.LSIDiv = RCC_LSI_DIV1;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
 RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV4;
 RCC_OscInitStruct.PLL.PLLM = 3;
 RCC_OscInitStruct.PLL.PLLN = 12;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
 RCC_OscInitStruct.PLL.PLLFRACN = 4096;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief CRC Initialization Function
 * None
 * @retval None
 */
static void MX_CRC_Init(void)
{

 /* USER CODE BEGIN CRC_Init 0 */

 /* USER CODE END CRC_Init 0 */

 /* USER CODE BEGIN CRC_Init 1 */

 /* USER CODE END CRC_Init 1 */
 hcrc.Instance = CRC;
 hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;
 hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;
 hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;
 hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;
 hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
 if (HAL_CRC_Init(&hcrc) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN CRC_Init 2 */

 /* USER CODE END CRC_Init 2 */

}

 

 

the ILI9341.c file:

 

// Call this function after ILI9341_SetWindow
// This function is non blocked
// The variable for Callback is open. User should set by himself
void ILI9341_DrawBitmap(uint16_t w, uint16_t h, uint8_t *s)
{
	// Enable to access GRAM
	LCD_WR_REG(0x2c);

	DC_H();
#if 0
	__HAL_SPI_DISABLE(&hspi1);
	hspi1.Instance->CR2 |= SPI_DATASIZE_16BIT; // Set 16 bit mode
	__HAL_SPI_ENABLE(&hspi1);
#endif
	ConvHL(s, (int32_t)w*h*2);
	HAL_SPI_Transmit_DMA(&hspi1, (uint8_t*)s, w * h *2); <= Runs in HardFault_Handler
#if 0
	__HAL_SPI_DISABLE(&hspi1);
	hspi1.Instance->CR2 &= ~(SPI_DATASIZE_16BIT); // Set 8 bit mode
	__HAL_SPI_ENABLE(&hspi1);
#endif
}

 

HAL_SPI_Transmit_DMA runs in HardFault_Handler...

What is wrong with my SPI1 Configuration?
Must i enable DMA?  And how can i enable The DMA for SPI1?

 

Thank you,

Daniel

 

This topic has been closed for replies.
Best answer by Andrew Neil

@Sany wrote:

after a lot of tests, it's working.


Great - now please mark the solution:
https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

 


@Sany wrote:

now i have a other problem, .


Please start a separate thread for a different question. You can always include a link to this one, for reference, if it helps.

Give a link here to your new thread - so that people can find it.

7 replies

Andrew Neil
Super User
December 17, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Sany
SanyAuthor
Associate III
December 17, 2024

Thank you, but i found out, the HardFault_Handler is called by

HAL_SPI_Transmit_DMA(&hspi1, (uint8_t*)s, w * h *2);

i think, SPI1 is not correctly configured, but i have a problem with my configuration of GPDMA1...

Andrew Neil
Super User
December 17, 2024

So the techniques presented should allow you to find where, exactly, the Fault occurs, and what Fault, exactly, it is ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.